This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:sigmastudiov2:modules:basic:minvaluehold [10 May 2021 06:03] – [Configurable Parameters] Nikhin Shetty | resources:tools-software:sigmastudiov2:modules:basic:minvaluehold [13 Sep 2022 11:33] (current) – Updates Image Angu Sewa | ||
---|---|---|---|
Line 2: | Line 2: | ||
====== Min Value Hold ====== | ====== Min Value Hold ====== | ||
\\ | \\ | ||
- | {{: | + | {{: |
===== Description ===== | ===== Description ===== | ||
The MinValueHold block monitors one (or more) input(s) and routes the minimum value of the input to the output. This block hold's the min value while the control input is 1 and reset the min value while the control input is 0. | The MinValueHold block monitors one (or more) input(s) and routes the minimum value of the input to the output. This block hold's the min value while the control input is 1 and reset the min value while the control input is 0. |