Wiki

The most recent version of this page is a draft.DiffThis version (10 Feb 2021 13:09) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Min Value Hold


Description

The MinValueHold block monitors one (or more) input(s) and routes the minimum value of the input to the output. This block held's the min value while the control input is 1 and reset the min value while the control input is 0.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
MinValueHold Yes YesYes Yes


Pins

Input

NameTypeDescription
ResetControlResets the minimum value
Input0AudioInput channel 0

Output

NameTypeDescription
Output0AudioOutput channel 0


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
NumChannels1 20Number of input and output channels. Change in this value requires re-compilation


DSP Parameters

No DSP parameters

/srv/wiki.analog.com/data/pages/resources/tools-software/sigmastudiov2/modules/basic/minvaluehold.txt · Last modified: 10 May 2021 06:03 by Nikhin Shetty