Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [04 Feb 2020 10:29]
Sanjeeva Reddy Added an image
resources:tools-software:sigmastudiov2:modules:basic:maxvaluehold [13 Sep 2022 11:33]
Angu Sewa Updates Image
Line 2: Line 2:
 ====== Max Value Hold ====== ====== Max Value Hold ======
 \\ \\
-{{:​resources:​tools-software:​sigmastudiov2:​modules:​basic:​maxhold.png}}+{{:​resources:​tools-software:​sigmastudiov2:​modules:​basic:​maxholdnew.png?nolink}}
 ===== Description ===== ===== Description =====
 The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0. The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0.
 \\ \\
 ===== Targets Supported ===== ===== Targets Supported =====
-^Name^ADSP-214xx(Sample)^ADSP-214xx(Block)^ADSP-215xx/​ADSP-SC5xx(Sample)^ADSP-215xx/ADSP-SC5xx(Block)+^ Name            ^ ADSP-214xx ^ ADSP-215xx/​SC5xx ^ ADAU145x/146x 
-|MaxValueHoldYes Yes|Yes| Yes+------------------------------------------------------------ ​-------------------- ​-------------------------------- ​---------------------------- ​
-\\+|MaxValueHold| B/S | B/S | B/S |
 ===== Pins ===== ===== Pins =====
 ==== Input ==== ==== Input ====
 ^Name^Type^Description^ ^Name^Type^Description^
 +|------------------------------|------------------------------------------------------------|------------------------------|
 |Reset|Control|Resets the maximum value| |Reset|Control|Resets the maximum value|
-|Input0|Audio|Input channel ​0|+|Input<fc #​ff0000>​X</​fc>​| Audio |Input channel ​X| 
 +Note: 
 +     * <fc #​ff0000>​X</​fc>​ - Channel Index
 ==== Output ==== ==== Output ====
 ^Name^Type^Description^ ^Name^Type^Description^
-|Output0|Audio|Output channel ​0| +|------------------------------|------------------------------------------------------------|------------------------------| 
-\\+|Output ​|Audio |Output channel |
 ===== Configurable Parameters ===== ===== Configurable Parameters =====
 ^GUI Parameter Name^Default Value^Range^Function Description^ ^GUI Parameter Name^Default Value^Range^Function Description^
 +|------------------------------|---------------------------|----------------------------|----------------------------------------------------------|
 |NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation| |NumChannels|1| 20|Number of input and output channels. Change in this value requires re-compilation|
-\\ 
-===== DSP Parameters ===== 
-No DSP parameters 
 \\ \\
resources/tools-software/sigmastudiov2/modules/basic/maxvaluehold.txt · Last modified: 13 Sep 2022 11:33 by Angu Sewa