Wiki

This version is outdated by a newer approved version.DiffThis version (10 Feb 2021 13:09) was approved by Sanjeeva Reddy.

This is an old revision of the document!


Click here to return to the Basic page

Max Value Hold


Description

The MaxValueHold block monitors one (or more) input(s) and routes the max value of the input to the output. This block held's the max value while the control input is 1 and reset the max value while the control input is 0.

Targets Supported

NameADSP-214xx(Sample)ADSP-214xx(Block)ADSP-215xx/ADSP-SC5xx(Sample)ADSP-215xx/ADSP-SC5xx(Block)
MaxValueHold Yes YesYes Yes


Pins

Input

NameTypeDescription
ResetControlResets the maximum value
Input0AudioInput channel 0

Output

NameTypeDescription
Output0AudioOutput channel 0


Configurable Parameters

GUI Parameter NameDefault ValueRangeFunction Description
NumChannels1 20Number of input and output channels. Change in this value requires re-compilation


DSP Parameters

No DSP parameters

resources/tools-software/sigmastudiov2/modules/basic/maxvaluehold.1580808579.txt.gz · Last modified: 04 Feb 2020 10:29 by Sanjeeva Reddy