For this final example the full virtual analog synth is run on Core1 and the effects chain is run on Core 2.
Part of this example will run on core 2 so be sure to set the following #define in audio_system_config.h
or select that Faust will run on both cores 1 and 2 when using the bare metal project wizard.
#define USE_FAUST_ALGORITHM_CORE2 TRUE
Multiple examples for the SHARC audio module have been put together and hosted on github. In order to successfully run this example, please clone this repository.
For this particular example workflow, we will be looking at the virtualAnalog example from the git repository.
Multiple examples for the SHARC audio module have been put together and hosted on github. In order to successfully run this example, please clone this repository.
For this particular example workflow, we will be looking at the virtualAnalog example from the git repository.
The block diagram button can be used to generate a hierarchical block diagram for an algorithm. This block diagram is hierarchical. Here are a few of the hierarchical levels:
The block diagram button can be used to generate a hierarchical block diagram for an algorithm. This block diagram is hierarchical. Here are a few of the hierarchical levels:
Export/compile to a specific platform
button sam
sam-source-poly-1
(core 1) or sam-source-midi
(core 2) and then Export:fast_pow2.h
samFaustDSP.cpp
samFaustDSP.h
Function | MIDI CC | Module | Type | Notes |
---|---|---|---|---|
Tune | 47 | 1 - Controllers | knob | Master tuning |
Glide | 5 | 1 - Controllers | knob | Portamento time |
Modulation Mix | 48 | 1 - Controllers | knob | Modulation mix between OSC3 and Noise |
Oscillator Modulation | 22 | 2 - Oscillator Bank | switch | Enable modulation control of OSC frequencies |
OSC 1 Range | 23 | 2 - Oscillator Bank | knob | OSC 1 range |
OSC 1 Detune | 24 | 2 - Oscillator Bank | knob | OSC 1 detuning |
OSC 1 Waveform | 25 | 2 - Oscillator Bank | knob | OSC 1 waveform shape |
OSC 2 Range | 28 | 2 - Oscillator Bank | knob | OSC 2 range |
OSC 2 Detune | 29 | 2 - Oscillator Bank | knob | OSC 2 detuning |
OSC 2 Waveform | 30 | 2 - Oscillator Bank | knob | OSC 2 waveform shape |
OSC 3 Range | 33 | 2 - Oscillator Bank | knob | OSC 3 range |
OSC 3 Detune | 34 | 2 - Oscillator Bank | knob | OSC 3 detuning |
OSC 3 Waveform | 35 | 2 - Oscillator Bank | knob | OSC 3 waveform shape |
OSC 3 Control | 9 | 2 - Oscillator Bank | switch | OSC 3 as a control signal or as an audio source |
OSC 1 Amp | 26 | 3 - Mixer | knob | OSC 1 gain |
Osc1 mixer switch | 12 | 3 - Mixer | switch | OSC 1 enable |
OSC 2 Amp | 31 | 3 - Mixer | knob | OSC 2 gain |
Osc2 mixer switch | 14 | 3 - Mixer | switch | OSC 2 enable |
OSC3 Amp | 36 | 3 - Mixer | knob | OSC 3 gain |
OSC3 mixer switch | 17 | 3 - Mixer | switch | OSC 3 enable |
External Input amp | 27 | 3 - Mixer | knob | Extrenal input gain |
External Input mixer switch | 13 | 3 - Mixer | switch | External input enable |
Noise Amp | 32 | 3 - Mixer | knob | Noise gain |
Noise mixer switch | 15 | 3 - Mixer | switch | Noise Enable |
White/pink toggle | 16 | 3 - Mixer | switch | Noise pink/white |
Filter Modulation Enable | 19 | 4 - Filter | switch | Enable modulation control of the filter cutoff frequency |
---|---|---|---|---|
Keyboard Range | 38 | 4 - Filter | knob | Add keyboard control of the filter cutoff frequency |
Cutoff Frequency | 74 | 4 - Filter | knob | Filter cutoff frequency |
Emphasis | 37 | 4 - Filter | knob | Filter Resonance (Q) |
Amount of Contour | 39 | 4 - Filter | knob | Amount of envelope generator |
Attack Time | 40 | 4 - Filter | knob | VCF envelope generator attack time |
Decay Time | 41 | 4 - Filter | knob | VCF envelope generator decay time |
Sustain Level | 42 | 4 - Filter | knob | VCF envelope generator sustain level |
Attack Time | 43 | 5 - Loudness Contour | knob | VCA envelope generator attack time |
Decay Time | 44 | 5 - Loudness Contour | knob | VCA envelope generator decay time |
Sustain Level | 45 | 5 - Loudness Contour | knob | VCA envelope generator sustain level |
Decay | 20 | 6 - Keyboard | switch | Enables using the decay stage as a release stage |
Glide | 65 | 6 - Keyboard | switch | Enable portamento |
Pitch Wheel | pitchWheel | 6 - Keyboard | knob | Pitch Wheel |
Mod Wheel | 1 | 6 - Keyboard | knob | Modulation Wheel control |
Sustain | 64 | midi sustain foot pedal | switch | Note sustain, preempts the VCF/VCA release stage |
Master Volume | 7 | 5 - Output | knob | Master volume |
Function | MIDI CC | Module | Type |
---|---|---|---|
Invert | 49 | Flanger | knob |
Enable | 102 | Flanger | switch |
Delay | 50 | Flanger | knob |
Rate | 51 | Flanger | knob |
Depth | 52 | Flanger | knob |
Feedback | 53 | Flanger | knob |
Wave Shape | 54 | Flanger | knob |
Delay | 55 | Chorus | knob |
Enable | 103 | Chorus | switch |
Rate | 56 | Chorus | knob |
Depth | 57 | Chorus | knob |
Deviation | 58 | Chorus | knob |
enable | 105 | Echo | switch |
Delay Portamento | 60 | Echo | knob |
Delay | 61 | Echo | knob |
Warp | 62 | Echo | knob |
Feedback | 2 | Echo | knob |
Amp | 75 | Echo | knob |
Feedback sm? | 76 | Echo | knob |
Damp | 3 | Reverb | knob |
Enable | 104 | Reverb | switch |
Room Size | 4 | Reverb | knob |
Wet Dry | 79 | Reverb | knob |
TouchOSC is a mobile app that can be used to create arbitrary GUIs that send MIDI values. TouchOSC is available for both iOS and Android. A TouchOSC configuration is provided for the Virtual Analog and Effects chain algorithms (virtualAnalog.touchOSC)
The Virtual Analog Page:
The Effects Chain Page: