Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:sharc-audio-module:faust:ex-work-virtual-analog [03 Oct 2018 22:28] Chad Wentworthresources:tools-software:sharc-audio-module:faust:ex-work-virtual-analog [15 Nov 2018 15:01] (current) – [MIDI Virtual Analog Synth (Core1) /Effects (Core 2)] Chad Wentworth
Line 2: Line 2:
  
 For this final example the full virtual analog synth is run on Core1 and the effects chain is run on Core 2. For this final example the full virtual analog synth is run on Core1 and the effects chain is run on Core 2.
-<WRAP important> +<WRAP round important> 
-Part of this example will run on core 2 so be sure to set the following #define in ''audio_system_config.h''+Part of this example will run on core 2 so be sure to set the following #define in ''audio_system_config.h'' or select that Faust will run on both cores 1 and 2 when using the [[resources:tools-software:sharc-audio-module:baremetal:project-wizard|bare metal project wizard]].
  
 <code c> <code c>
resources/tools-software/sharc-audio-module/faust/ex-work-virtual-analog.txt · Last modified: 15 Nov 2018 15:01 by Chad Wentworth