Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:fpga:docs:util_extract [11 Oct 2021 14:57]
Iulia Moldovan Edit footer
resources:fpga:docs:util_extract [13 Oct 2021 08:33]
Iulia Moldovan Edit footer
Line 1: Line 1:
-===== UTIL_EXTRACT =====+====== UTIL_EXTRACT ​======
  
 The UTIL_EXTRACT IP allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI_ADC_TRIGGER IP. The UTIL_EXTRACT IP allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI_ADC_TRIGGER IP.
  
-==== Configuration Parameters ====+ 
 +===== Configuration Parameters ​=====
  
 ^ Name ^ Description ^ Default Value^ ^ Name ^ Description ^ Default Value^
Line 9: Line 10:
 | ''​DATA_WIDTH''​ | Data width. It assumes the trigger is in bit (n*16)-1, with n being the channel number | NUM_OF_CHANNELS * 16 | | ''​DATA_WIDTH''​ | Data width. It assumes the trigger is in bit (n*16)-1, with n being the channel number | NUM_OF_CHANNELS * 16 |
  
-==== Interface ====+ 
 +===== Interface ​=====
  
 ^ Interface ^ Pin ^ Type ^ Description ^ ^ Interface ^ Pin ^ Type ^ Description ^
Line 22: Line 24:
 |              | ''​trigger_out''​ | ''​output''​ | Trigger output. Is an logic OR of the triggers from all the channels that are captured simulaneously | |              | ''​trigger_out''​ | ''​output''​ | Trigger output. Is an logic OR of the triggers from all the channels that are captured simulaneously |
  
-==== References ====+ 
 +===== References ​=====
   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​util_extract | UTIL_EXTRACT IP source code]] \\   * [[https://​github.com/​analogdevicesinc/​hdl/​tree/​master/​library/​util_extract | UTIL_EXTRACT IP source code]] \\
   * [[/​resources/​fpga/​docs/​arch | ADI Reference designs architecture ]] \\   * [[/​resources/​fpga/​docs/​arch | ADI Reference designs architecture ]] \\
  
-{{navigation HDL User Guide#axi_ip|AXI IP cores#​hdl|Main page#​tips|Using and modifying the HDL design}}+{{navigation HDL User Guide#ip_cores|IP cores#​hdl|Main page#​tips|Using and modifying the HDL design}}
resources/fpga/docs/util_extract.txt · Last modified: 13 Oct 2021 08:33 by Iulia Moldovan