Wiki

This version is outdated by a newer approved version.DiffThis version (11 Oct 2021 15:52) was approved by Adrian Costina.The Previously approved version (14 Jan 2021 05:24) is available.Diff

This is an old revision of the document!


UTIL_EXTRACT

The UTIL_EXTRACT IP allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI_ADC_TRIGGER IP.

Configuration Parameters

Name Description Default Value
NUM_OF_CHANNELS Number of channels 2
DATA_WIDTH Data width. It assumes the trigger is in bit (n*16)-1, with n being the channel number NUM_OF_CHANNELS * 16

Interface

Interface Pin Type Description
Clock
clk input Clock input. Should be synchronous to the input and the output data
Data Input
data_in input[DATA_WIDTH-1:0] Input data from the FIFO. Will replace each trigger bit with the sign extended version of the data. It should be data from the output of the variable fifo
data_in_trigger input[DATA_WIDTH-1:0] Data from which the trigger is extracted. It should be data from the input of the variable fifo
data_in_valid input Valid for the input data
Data Output
data_out output[DATA_WIDTH-1:0] Data without the embedded trigger
trigger_out output Trigger output. Is an logic OR of the triggers from all the channels that are captured simulaneously

References

resources/fpga/docs/util_extract.1633957070.txt.gz · Last modified: 11 Oct 2021 14:57 by Iulia Moldovan