This is an old revision of the document!
The AXI_DAC_INTERPOLATE IP allows interpolation of the input data by 10/100/1000/10000/100000, with filtering and arbitrary zero-hold interpolation.
Name | Description | Default Value |
---|---|---|
CORRECTION_DISABLE | Disable scale correction of the CIC output | 1 |
Interface | Pin | Type | Description |
---|---|---|---|
Clock | |||
dac_clk | input | Clock input | |
Reset | |||
dac_rst | input | Reset, synchronous on the dac_clk clock domain | |
Data Inputs | |||
dac_data_a | input[15:0] | Analog data for channel A | |
dac_data_b | input[15:0] | Analog data for channel B | |
dac_data_valid_a | input | Data valid signal for channel A | |
dac_data_valid_b | input | Data valid signal for channel B | |
Interpolated Outputs | |||
dac_int_data_a | output[15:0] | Interpolated data for channel A | |
dac_int_data_b | output[15:0] | Interpolated data for channel B | |
dac_int_valid_a | output | Data valid for channel A | |
dac_int_valid_b | output | Data valid for channel B | |
AXI_S_MM interface | |||
s_axi_* | Standard AXI Slave Memory Map interface |
For some applications the maximum sampling rate of the DAC is too high and leads to a bad utilization of the memory or USB bandwidth. In order to avoid that, the interpolation IP can be used.
The interpolation block allows interpolation by 10, 100, 1000, 10000,100000 with filtering. The filtering is implemented using a FIR compensation filter (interpolation by 2) for the CIC and a 6 stage CIC interpolation filter allowing interpolation by 5/50/500/5000/50000.
At the end of the filter blocks, there is an arbitrary interpolation zero-order hold block which holds the value for a configurable number of samples.
Address | Bits | Name | Type | Description | |
DWORD | BYTE | ||||
0x0000 | 0x0000 | REG_VERSION | Version Register | ||
---|---|---|---|---|---|
[31:0] | VERSION | RO | Version number | ||
0x0001 | 0x0004 | REG_SCRATCH | Scratch Register | ||
[31:0] | SCRATCH | RW | Scratch register | ||
0x0010 | 0x0040 | REG_ARBITRARY_INTERPOLATION_RATIO_A | Control Arbitrary Interpolation Ratio for Channel A | ||
[31:0] | FILTERED_INTERPOLATION_RATIO | RW | Set the arbitrary zero-order hold interpolation ratio at the end of the interpolation chain | ||
0x0011 | 0x0044 | REG_INTERPOLATION_RATIO_A | Control Filtered Interpolation for Channel A | ||
[2:0] | FILTERED_INTERPOLATION_RATIO | RW | Enables the filtered interpolation: 0: No filtered interpolation 1: Interpolation by 10. Result should be corrected by a 1.531 factor 2: Interpolation by 100. Result should be corrected by a 1.168 factor 3: Interpolation by 1000. Result should be corrected by a 1.783 factor 6: Interpolation by 10000. Result should be corrected by a 1.360 factor 7: Interpolation by 100000. Result should be corrected by a 1.038 factor default: No filtered interpolation |
||
0x0012 | 0x0048 | REG_ARBITRARY_INTERPOLATION_RATIO_B | Control Arbitrary Interpolation Ratio for Channel B | ||
[31:0] | FILTERED_INTERPOLATION_RATIO | RW | Set the arbitrary zero-order hold interpolation ratio at the end of the interpolation chain | ||
0x0013 | 0x004c | REG_INTERPOLATION_RATIO_B | Control Filtered Interpolation for Channel B | ||
[2:0] | FILTERED_INTERPOLATION_RATIO | RW | Enables the filtered interpolation: 0: No filtered interpolation 1: Interpolation by 10. Result should be corrected by a 1.531 factor 2: Interpolation by 100. Result should be corrected by a 1.168 factor 3: Interpolation by 1000. Result should be corrected by a 1.783 factor 6: Interpolation by 10000. Result should be corrected by a 1.360 factor 7: Interpolation by 100000. Result should be corrected by a 1.038 factor default: No filtered interpolation |
||
0x0014 | 0x0050 | REG_FLAGS | Control Flags | ||
[0] | SUSPEND_TRANSFER | RW | If set to 1, the interpolation filters are in reset and no data is requested from the DMA. Can be used to synchronize data transfer from two different DMAs. | ||
0x0015 | 0x0054 | REG_CONFIG | Configuration Register | ||
[1] | CORRECTION_ENABLE_B | RW | If set to 1, correction is enabled on channel B. The input data will be multiplied with the value from the CORRECTION_COEFFICIENT_B register. | ||
[0] | CORRECTION_ENABLE_A | RW | If set to 1, correction is enabled on channel A. The input data will be multiplied with the value from the CORRECTION_COEFFICIENT_A register. | ||
0x0016 | 0x0058 | REG_CORRECTION_COEFFICIENT_A | Correction Coefficient A | ||
[15:0] | CORRECTION_COEFFICIENT | RW | Scale correction (if equipped) coefficient for channel A. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. | ||
0x0017 | 0x005c | REG_CORRECTION_COEFFICIENT_B | Correction Coefficient B | ||
[15:0] | CORRECTION_COEFFICIENT | RW | Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification. |