This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:pzsdr:power-and-sequencing [26 Aug 2016 23:22] – [Fixing the problem for HR Banks 12 and 13] Neil Wilson | resources:eval:user-guides:pzsdr:power-and-sequencing [03 Jan 2021 21:46] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 130: | Line 130: | ||
* 1 PZSDR Board. | * 1 PZSDR Board. | ||
* 1 microSD card (with appropriate image). | * 1 microSD card (with appropriate image). | ||
- | * 1 [[http:// | + | * 1 [[adi>en/ |
{{ : | {{ : | ||
* 1 Custom Adapter for the USB-SDP-CABLEZ. | * 1 Custom Adapter for the USB-SDP-CABLEZ. | ||
{{ : | {{ : | ||
- | * [[http:// | + | * [[adi>en/ |
- | * [[http:// | + | * [[adi>en/ |
===Software Setup=== | ===Software Setup=== | ||
Line 185: | Line 185: | ||
{{: | {{: | ||
- | =====Software | + | =====Software - Input Voltage Range Determination and Setting===== |
The following provides a detailed overview on how the ADM1166 input voltage ranges are calculated and programmed to account for input and output ZYNQ voltage settings, ADM116 power sequencer input voltage ranges etc. | The following provides a detailed overview on how the ADM1166 input voltage ranges are calculated and programmed to account for input and output ZYNQ voltage settings, ADM116 power sequencer input voltage ranges etc. | ||
Line 303: | Line 303: | ||
| VMGTAVCC | | VMGTAVCC | ||
| VMGTAVTT | | VMGTAVTT | ||
- | | VCCO (HR Bank) | Mid-Range| 1.140 V | 3.465 V | 2.671 V | 3.348 V | 2.500 V | 6.000 V | | + | | VCCO (HR Bank) | Mid-Range| 1.140 V | 3.465 V | 2.431 V | 3.043 V | 2.500 V | 6.000 V | |
- | | VCCO (HP Bank) | Ultralow | 1.140 V | 1.890 V | 0.808 V | 1.356 V | 0.573 V | 1.375 V | | + | | VCCO (HP Bank) | Ultralow | 1.140 V | 1.890 V | 0.748 V | 1.192 V | 0.573 V | 1.375 V | |
Line 342: | Line 342: | ||
JX_VCCO_12 | JX_VCCO_12 | ||
- | {{: | + | {{: |
JX_VCCO_13 | JX_VCCO_13 | ||
- | {{: | + | {{: |
JX_VCCO_33_34 | JX_VCCO_33_34 | ||
Line 356: | Line 356: | ||
==== But wait… the calculated tables are slightly different from the software values! ==== | ==== But wait… the calculated tables are slightly different from the software values! ==== | ||
- | The thresholds are programmed using 8-bit resolution so the program was written to be as close to the UV or OV threshold, without restricting the range at all. | + | The thresholds are programmed using 8-bit resolution so the program was written to be as close to the UV or OV threshold, without restricting the range, and in some cases adding a small amount of headroom. |
==== This looks great, but, I need to change some settings for my custom carrier. ==== | ==== This looks great, but, I need to change some settings for my custom carrier. ==== | ||
- | Thinking of modifying the VH Thresholds? Be very careful! | + | |
+ | Thinking of modifying the VH Thresholds? | ||
+ | |||
+ | {{: | ||
Thinking of modifying other settings? Still be careful! | Thinking of modifying other settings? Still be careful! | ||
- | This is not to say DON’T change settings, merely… think twice, then think twice more, then program once. | + | This is not to say DON’T change settings, merely… think twice, then think twice more, then program once. The worst thing to happen is to have a board with no power and no way to reprogram the threshold you just changed. |
+ | |||
+ | |||
+ | |||
==== I programmed twice and thought once.==== | ==== I programmed twice and thought once.==== | ||
Line 371: | Line 378: | ||
==== Is there a default file I can load? ==== | ==== Is there a default file I can load? ==== | ||
The default file that comes pre-loaded when you order hardware can be found on [[https:// | The default file that comes pre-loaded when you order hardware can be found on [[https:// | ||
+ | |||
+ | This file is also updated on occasion to include new features, tweaks or other items which pop up as systems are developed. | ||
{{navigation PicoZed_SDR# | {{navigation PicoZed_SDR# |