Wiki

This version (09 Jan 2021 00:42) was approved by Robin Getz.The Previously approved version (26 Jan 2014 23:17) is available.Diff

ADIS1636x/40x EVALUATION ON THE EVAL-ADIS

OVERVIEW

The ADIS16362 is a high-performance IMU that uses a serial peripheral interface for data communications. This interface enables direct connection with a large variety of embedded processor products. This electrical connection typically only requires 5 I/O lines for synchronous data collection, as shown in the following figure:

This Wiki will cover all members of the ADIS1636x family: ADIS16360 ADIS16362, ADIS16364, ADIS16365, ADIS16367, ADIS16400 ADIS16405, ADIS16407.

ADIS1636x/PCB & ADIS1640x/PCBZ BREAKOUT BOARDS

For those who are on a tight timeline, connecting the ADIS1636xBMLZ or ADIS1640xBMLZ to an embedded controller will provide the most flexibility in developing application firmware and will more closely reflect the final system design. For example, the ADIS16362/PCBZ is the breakout board for the ADIS16362 and may provide assistance in the process of hooking it up to an existing embedded processor system. Also see the following breakout board pages:

ADIS16360/PCBZ

ADIS16362/PCBZ

ADIS16364/PCBZ

ADIS16365/PCBZ

ADIS16367/PCBZ

ADIS16400/PCBZ

ADIS16405/PCBZ

ADIS16407/PCBZ

ADIS16IMU1/PCBZ BREAKOUT BOARD

The interface board that comes with ADIS1636x/PCBZ or ADIS1640x/PCBZ orders has two 12-pin connectors: J1 contains the power, ground and SPI signals while J2 contains the DIOx pins (including data-ready). The ADIS16IMU1/PCBZ provides access to all of these functions through one 16-pin connector, which simplifies cabling requirements. Click on the following link for more information on the ADIS16IMU1/PCBZ:

ADIS16IMU1/PCB Wiki Guide

In addition to offering the convenience of one 16-pin connector, the ADIS16IMU1/PCBZ also offers M2x0.4mm tapped holes and machine screws to attach any ADIS1636xBMLZ or ADIS1640xBMLZ product to it.

NOTE: Order ADIS16360BMLZ, ADIS16362BMLZ, ADIS16364BMLZ, ADIS16365BMLZ, ADIS16367BMLZ, ADIS16400BMLZ, ADIS16405BMLZ or ADIS16407BMLZ separately, as they are not included with the ADIS16IMU1/PCBZ.

EVAL-ADIS: PC EVALUATION

For those who would prefer to perform PC-based evaluation of the ADIS1636x or ADIS1640x products, before developing their own embedded system, the EVAL-ADIS is the appropriate system to use. The remainder of this Wiki site will focus on PC-based evaluation with the EVAL-ADIS system. Here is a list of equipment required for this:

EVAL-ADISZ

ADIS16362BMLZ

NOTE: Substitute ADIS16360BMLZ, ADIS16364BMLZ, ADIS16365BMLZ, ADIS16367BMLZ, ADIS16400BMLZ, ADIS16405BMLZ or ADIS16407BMLZ for the ADIS16362BMLZ, as needed for specific application requirements.

EQUIPMENT LIST

SYSTEM REQUIREMENTS

Windows XP, Vista, 7

.NET Framework 3.5

NOTE: Newer versions of the .NET framework do not currently support the IMU Evaluation software package.

PHYSICAL SETUP

The ADIS16362/PCBZ includes one interface PCB, which requires two M2 or 2-56 machine screws to secure the baseplate to the system printed circuit board. The ADIS16362 product family is approximately 22 mm × 32 mm × 24 mm and provides a flexible connector interface that enables multiple mounting orientation options. Set the interface PCB aside, as it is not used for connecting the ADIS16362 to the EVAL-ADIS.

NOTE: The machine screws that come with the EVAL-ADIS can have a moderate impact on local magnetic fields. For those who need the best performance out of the magnetometer solution, consider replacing them with machine screws that are made out of aluminum or other non-ferrous materials.

NOTE: Do not plug the EVAL-ADIS into the USB cable at this stage of the setup. Wait until the software installation is complete.

Step #1

The ADIS16362 installs directly into the J4 connector of the EVAL-ADIS The B-holes on the EVAL-ADIS, are used for ADIS16362 mounting and marked in the picture below.

WARNING: Make sure that the connector is in proper alignment before pressing it in. Misalignment can cause pin damage and exposure to harmful conditions.

Step #2

The ADIS16362 installation, is a simple two-step process:

1. Secure the baseplate using 2 M2 x 0.4mm x 6mm machine screws and the B-holes on the EVAL-ADIS.

2. Press the connector into its mate.

For removal, 1. Gently pry the connector from its mate using a small slot

screwdriver. 2. Remove the screws and lift the part up.

Never attempt to unplug the connector by pulling on the plastic case or baseplate. Although the flexible connector is very reliable in normal operation, it can break when subjected to unreasonable handling. When broken, the flexible connector cannot be repaired.

Step #3

The following picture shows JP1 in the +5V position required for the ADIS16362 product family sensors. Note the JP1 jumper (factory-default) setting on the EVAL-ADIS is +3.3V. The power management system provides jumper selection for three device under test (DUT) power options: 5 V (USB), 3.3 V, and an external power option. The 5 V option provides access to the USB’s 5 V supply voltage for the DUT, and the 3.3 V option uses a linear regulator, 400 μF of bulk capacitance, and a soft start circuit to manage transient currents on the USB port.

NOTE: If JP1 is left on +3.3V, all outputs may not respond and will appear to be saturated in one direction or the other. See the following picture for an example of this behavior.

IMU EVALUATION SOFTWARE OVERVIEW

The EVAL-ADIS2 has been superseded by the EVAL-ADIS-FX3 and is no longer supported.
This guide assumes that you've connected your vibration sensor to the EVAL-ADIS2, drivers were successfully installed on your PC, and you've downloaded the correct software for your sensor. We recommend reviewing the Hardware User Guide before continuing.

Software Downloads

Click here to download the latest version of the IMU Evaluation software.

Click here to download the latest drivers for the EVAL-ADIS2.

This application requires Microsoft .NET 3.5 to be installed and enabled on the host PCs running Windows 10. Additional information on enabling .NET 3.5 can be found here.

EVAL-ADIS2 IMU Evaluation Software Overview

The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.

This guide builds upon the EVAL-ADIS2 Hardware User Guide and assumes that you've installed the necessary drivers and software.

Using the EVAL-ADIS2 IMU Evaluation Software

Main Window

Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.

The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.

The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.

- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.

- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.

- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.

- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.

- The Tools option calls a sub-menu that displays USB diagnostic information.

- The About option provides more detailed software revision information.

The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).

The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).

Register Access

The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.

The color-coded image below is referenced in the following section.

The purple box sorts each set of registers into a standard category. The available categories are:

- Control/Status - General sensor configuration, alarm, and metadata registers

- Output - Inertial sensor output registers

- Calibration - User offset and misc. calibration registers

The calibration register section mentioned above is separate from the factory calibration registers and procedures!

The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.

The green box identifies the read/write control options for the current register selection.

Registers must be written in hexadecimal format!

The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.

The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.

The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.

The Register Access form always writes to both the upper and lower bytes of a given register. When writing to a register, make sure to include the desired 16-bit value in hexadecimal format before clicking the Write Register button.
Data Capture

The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.

The color-coded image below is referenced in the following section.

The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.

The section highlighted in green allows for customizing the file name and location of the resultant .csv files.

The section highlighted in yellow identifies the data stream configuration options.

- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor

- Sample Rate - The instantaneous data ready rate as measured by the evaluation board

- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate

- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file

- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second

Software Revision History

Click to display ⇲

Click to hide ⇱

REVISION RELEASE DATE SUMMARY OF UPDATES
v1.14.3 8/5/15 Adjust ADIS16210 registers to match recent datasheet updates
v1.14.2 TBD Internal update
v1.14.1 TBD Internal update
v1.14.0 3/2/15 Internal update
v1.13.0 Internal update
v1.12.0 Internal update
v1.11.1 4/9/14 Updated Magnetometer recorder in the Main Menu for consistency across the ADIS16405, ADIS16407, ADIS16448 and ADIS16488
v1.10.1 12/9/13 Address reported issue with SYS_E_FLAG register missing from ADIS16485 and ADIS16488 Register Access Menu
v1.10.0 11/1/13 Add support for the ADIS16137
Fix register access (GPIO_CTRL) in ADIS16209
v1.9.8 8/27/2013 Corrected a number of register definition issues on the ADIS16480
v1.9.7 8/21/2013 Corrected scale factors associated with GYRO_OUT/GYRO_OUT2 registers in the ADIS16133/5
v1.9.6 N/A Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/40x
NOTE: This version was not posted online, but these updates are in current versions
v1.9.5 N/A Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445
Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448
NOTE: This version was not posted online, but these updates are in current versions
v1.9.4 N/A Enabled support for using an external clock on the ADIS16405
NOTE: This version was not posted online, but these updates are in current versions
v1.9.3 3/18/2013 Added support for the ADIS16400 and ADIS16405
v1.9.2 2/18/2013 Changed the separation “de-limit” in the data captures file from a comma to a semicolon
v1.9.0 1/16/2013 Added support for the ADIS16209 and ADIS16210
Corrected scale factors associated with the xDELTVEL_xxx registers in the ADIS16480/5
v1.8.1 12/18/2013 Corrected a data capture error, which was observed in the ADIS16448, but could have impacted other products
v1.8.0 11/8/2013 Added support for external clock use
Added support for the ADIS16266
v1.7.0 10/1/12 Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367
Corrected a scaling issue for those who use “Turkey” as their regional setting.
NOTE: Some sensitivity was still observed; some users in Turkey may need to change the regional setting to fully address.
v1.6.0 9/3/12 Added support for the ADIS16300 and ADIS16305
v1.5.0 8/22/12 Added support for the ADIS16445
v1.4.0 7/18/12 Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334
v1.3.0 N/A Internal updates
NOTE: This version was not posted online, but these updates are in current versions
v1.2.0 5/28/2012 Added support for the ADIS16480
Added 3-D viewer for ADIS16480 demonstration
v1.1.1 5/4/2012 Updated register names for ADIS16448/ADIS16485 to match datasheet names
Data Capture: changed “Cancel” button to “Stop”
v1.1.0 4/6/2012 Added support for the ADIS16485
Improvements to Waveform Recorder appearance
v1.0.1 3/27/2012 Addressed issue to enable correct register values in the Register Access menu
v1.0.0 3/24/2012 Initial Release

USB Driver Installation

The EVAL-ADIS2 has been superseded by the EVAL-ADIS-FX3 and is no longer supported.
This guide assumes that you've connected your vibration sensor to the EVAL-ADIS2, drivers were successfully installed on your PC, and you've downloaded the correct software for your sensor. We recommend reviewing the Hardware User Guide before continuing.

Software Downloads

Click here to download the latest version of the IMU Evaluation software.

Click here to download the latest drivers for the EVAL-ADIS2.

This application requires Microsoft .NET 3.5 to be installed and enabled on the host PCs running Windows 10. Additional information on enabling .NET 3.5 can be found here.

EVAL-ADIS2 IMU Evaluation Software Overview

The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.

This guide builds upon the EVAL-ADIS2 Hardware User Guide and assumes that you've installed the necessary drivers and software.

Using the EVAL-ADIS2 IMU Evaluation Software

Main Window

Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.

The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.

The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.

- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.

- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.

- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.

- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.

- The Tools option calls a sub-menu that displays USB diagnostic information.

- The About option provides more detailed software revision information.

The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).

The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).

Register Access

The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.

The color-coded image below is referenced in the following section.

The purple box sorts each set of registers into a standard category. The available categories are:

- Control/Status - General sensor configuration, alarm, and metadata registers

- Output - Inertial sensor output registers

- Calibration - User offset and misc. calibration registers

The calibration register section mentioned above is separate from the factory calibration registers and procedures!

The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.

The green box identifies the read/write control options for the current register selection.

Registers must be written in hexadecimal format!

The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.

The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.

The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.

The Register Access form always writes to both the upper and lower bytes of a given register. When writing to a register, make sure to include the desired 16-bit value in hexadecimal format before clicking the Write Register button.
Data Capture

The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.

The color-coded image below is referenced in the following section.

The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.

The section highlighted in green allows for customizing the file name and location of the resultant .csv files.

The section highlighted in yellow identifies the data stream configuration options.

- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor

- Sample Rate - The instantaneous data ready rate as measured by the evaluation board

- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate

- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file

- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second

Software Revision History

Click to display ⇲

Click to hide ⇱

REVISION RELEASE DATE SUMMARY OF UPDATES
v1.14.3 8/5/15 Adjust ADIS16210 registers to match recent datasheet updates
v1.14.2 TBD Internal update
v1.14.1 TBD Internal update
v1.14.0 3/2/15 Internal update
v1.13.0 Internal update
v1.12.0 Internal update
v1.11.1 4/9/14 Updated Magnetometer recorder in the Main Menu for consistency across the ADIS16405, ADIS16407, ADIS16448 and ADIS16488
v1.10.1 12/9/13 Address reported issue with SYS_E_FLAG register missing from ADIS16485 and ADIS16488 Register Access Menu
v1.10.0 11/1/13 Add support for the ADIS16137
Fix register access (GPIO_CTRL) in ADIS16209
v1.9.8 8/27/2013 Corrected a number of register definition issues on the ADIS16480
v1.9.7 8/21/2013 Corrected scale factors associated with GYRO_OUT/GYRO_OUT2 registers in the ADIS16133/5
v1.9.6 N/A Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/40x
NOTE: This version was not posted online, but these updates are in current versions
v1.9.5 N/A Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445
Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448
NOTE: This version was not posted online, but these updates are in current versions
v1.9.4 N/A Enabled support for using an external clock on the ADIS16405
NOTE: This version was not posted online, but these updates are in current versions
v1.9.3 3/18/2013 Added support for the ADIS16400 and ADIS16405
v1.9.2 2/18/2013 Changed the separation “de-limit” in the data captures file from a comma to a semicolon
v1.9.0 1/16/2013 Added support for the ADIS16209 and ADIS16210
Corrected scale factors associated with the xDELTVEL_xxx registers in the ADIS16480/5
v1.8.1 12/18/2013 Corrected a data capture error, which was observed in the ADIS16448, but could have impacted other products
v1.8.0 11/8/2013 Added support for external clock use
Added support for the ADIS16266
v1.7.0 10/1/12 Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367
Corrected a scaling issue for those who use “Turkey” as their regional setting.
NOTE: Some sensitivity was still observed; some users in Turkey may need to change the regional setting to fully address.
v1.6.0 9/3/12 Added support for the ADIS16300 and ADIS16305
v1.5.0 8/22/12 Added support for the ADIS16445
v1.4.0 7/18/12 Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334
v1.3.0 N/A Internal updates
NOTE: This version was not posted online, but these updates are in current versions
v1.2.0 5/28/2012 Added support for the ADIS16480
Added 3-D viewer for ADIS16480 demonstration
v1.1.1 5/4/2012 Updated register names for ADIS16448/ADIS16485 to match datasheet names
Data Capture: changed “Cancel” button to “Stop”
v1.1.0 4/6/2012 Added support for the ADIS16485
Improvements to Waveform Recorder appearance
v1.0.1 3/27/2012 Addressed issue to enable correct register values in the Register Access menu
v1.0.0 3/24/2012 Initial Release

IMU EVALUATION SOFTWARE GETTING STARTED

The EVAL-ADIS2 has been superseded by the EVAL-ADIS-FX3 and is no longer supported.
This guide assumes that you've connected your vibration sensor to the EVAL-ADIS2, drivers were successfully installed on your PC, and you've downloaded the correct software for your sensor. We recommend reviewing the Hardware User Guide before continuing.

Software Downloads

Click here to download the latest version of the IMU Evaluation software.

Click here to download the latest drivers for the EVAL-ADIS2.

This application requires Microsoft .NET 3.5 to be installed and enabled on the host PCs running Windows 10. Additional information on enabling .NET 3.5 can be found here.

EVAL-ADIS2 IMU Evaluation Software Overview

The IMU Evaluation Software is a Microsoft Windows (.NET) application that works in conjunction with the EVAL-ADIS2, in order to provide users with a PC-Based interface to most ADIS16xxx products. This platform enables observation of basic sensor functions, read/write access to all user-accessible registers, and full-rate data acquisition, which is synchronous with data production of each ADIS16xxx.

This guide builds upon the EVAL-ADIS2 Hardware User Guide and assumes that you've installed the necessary drivers and software.

Using the EVAL-ADIS2 IMU Evaluation Software

Main Window

Once the IMU Evaluation software loads, you should be presented with a window similar to the image shown below.

The image below has been color-coded to illustrate the different parts of the IMU Evaluation Software. These colored sections will be referred to in the following sections.

The drop-down menus highlighted in orange list additional features and utilities that make up the core functionality of the evaluation software.

- The Devices menu provides a list of supported products. Selecting a product from this list will configure the IMU evaluation software register map. Each device has a unique register map that must be selected to ensure proper sensor operation. The green box shows the active device. In this example, the ADIS16448 is selected.

- The Register Access option calls a sub-menu that lists all user-configurable registers available from the part number selected in the “Devices” drop-down menu. It also provides read/write access to each register.

- The Data Capture option calls a sub-menu designed to enable synchronous data logging from the selected device.

- The Demos option calls a 3-D visualization tool. This feature is only supported for the ADIS16480 and ADIS16448 devices.

- The Tools option calls a sub-menu that displays USB diagnostic information.

- The About option provides more detailed software revision information.

The purple box shows the primary, inertial output registers for the selected device. These values are updated in real-time after pressing the Read button (identified by a red box).

The yellow box shows three waveform recorder windows. Each window allows for plotting the three primary sensor types (gyroscopes, accelerometers, and magnetometers [if supported]). The top subplot displays gyroscope data, the middle plot displays accelerometer data and the bottom plot displays magnetometer data. Each plot color corresponds to the colors displayed in the “Output Registers” window (highlighted in purple).

Register Access

The Register Access window provides read and write access to all user-accessible registers listed in the selected device's datasheet. The image below shows a screenshot of the window.

The color-coded image below is referenced in the following section.

The purple box sorts each set of registers into a standard category. The available categories are:

- Control/Status - General sensor configuration, alarm, and metadata registers

- Output - Inertial sensor output registers

- Calibration - User offset and misc. calibration registers

The calibration register section mentioned above is separate from the factory calibration registers and procedures!

The section highlighted by the red box lists all of the registers in the selected category. Click on the register name to select a register for individual read/write access.

The green box identifies the read/write control options for the current register selection.

Registers must be written in hexadecimal format!

The Update Registers in Category button (shown in an orange box above) automatically reads all of the registers shown in the selected category (red box) and updates their contents in the GUI.

The section highlighted in yellow identifies provides a means of easily calling subroutines within the connected sensor. Clicking on a button is equivalent to writing a single-bit command to the respective register.

The Save Reg Settings to File programmatically reads and saves the contents of all of the registers in the current category into a *.csv (common-delimited) file. The Load Reg Settings from File button reads a target .csv file and attempts to write the saved values back into the sensor.

The Register Access form always writes to both the upper and lower bytes of a given register. When writing to a register, make sure to include the desired 16-bit value in hexadecimal format before clicking the Write Register button.
Data Capture

The Data Capture window only supports synchronous data acquisition and logging to a file on the host PC. Data samples are only read from the sensor when the data ready pin toggles, indicating that data is valid.

The color-coded image below is referenced in the following section.

The section highlighted in red lists all of the registers that are eligible for data capture. Checking the box next to each register indicates that the specified register values should be recorded once the data stream begins.

The section highlighted in green allows for customizing the file name and location of the resultant .csv files.

The section highlighted in yellow identifies the data stream configuration options.

- Record Length - The total number of samples to be captured. A sample is defined as a single “data valid” period as signaled by the data ready pin on the sensor

- Sample Rate - The instantaneous data ready rate as measured by the evaluation board

- Capture Time - The estimated data capture time in DD:HH:MM:SS format calculated based upon the instantaneous sample rate

- Add File Header - Selects whether a header displaying the contents of each column should be appended to the beginning of the .csv file

- Use Scaled Data - Signals to the software to convert the 16-bit values read from the sensor into a sign-adjusted (two's complement) scaled number. For example, when this option is enabled, be in units of degrees/second

Software Revision History

Click to display ⇲

Click to hide ⇱

REVISION RELEASE DATE SUMMARY OF UPDATES
v1.14.3 8/5/15 Adjust ADIS16210 registers to match recent datasheet updates
v1.14.2 TBD Internal update
v1.14.1 TBD Internal update
v1.14.0 3/2/15 Internal update
v1.13.0 Internal update
v1.12.0 Internal update
v1.11.1 4/9/14 Updated Magnetometer recorder in the Main Menu for consistency across the ADIS16405, ADIS16407, ADIS16448 and ADIS16488
v1.10.1 12/9/13 Address reported issue with SYS_E_FLAG register missing from ADIS16485 and ADIS16488 Register Access Menu
v1.10.0 11/1/13 Add support for the ADIS16137
Fix register access (GPIO_CTRL) in ADIS16209
v1.9.8 8/27/2013 Corrected a number of register definition issues on the ADIS16480
v1.9.7 8/21/2013 Corrected scale factors associated with GYRO_OUT/GYRO_OUT2 registers in the ADIS16133/5
v1.9.6 N/A Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/40x
NOTE: This version was not posted online, but these updates are in current versions
v1.9.5 N/A Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445
Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448
NOTE: This version was not posted online, but these updates are in current versions
v1.9.4 N/A Enabled support for using an external clock on the ADIS16405
NOTE: This version was not posted online, but these updates are in current versions
v1.9.3 3/18/2013 Added support for the ADIS16400 and ADIS16405
v1.9.2 2/18/2013 Changed the separation “de-limit” in the data captures file from a comma to a semicolon
v1.9.0 1/16/2013 Added support for the ADIS16209 and ADIS16210
Corrected scale factors associated with the xDELTVEL_xxx registers in the ADIS16480/5
v1.8.1 12/18/2013 Corrected a data capture error, which was observed in the ADIS16448, but could have impacted other products
v1.8.0 11/8/2013 Added support for external clock use
Added support for the ADIS16266
v1.7.0 10/1/12 Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367
Corrected a scaling issue for those who use “Turkey” as their regional setting.
NOTE: Some sensitivity was still observed; some users in Turkey may need to change the regional setting to fully address.
v1.6.0 9/3/12 Added support for the ADIS16300 and ADIS16305
v1.5.0 8/22/12 Added support for the ADIS16445
v1.4.0 7/18/12 Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334
v1.3.0 N/A Internal updates
NOTE: This version was not posted online, but these updates are in current versions
v1.2.0 5/28/2012 Added support for the ADIS16480
Added 3-D viewer for ADIS16480 demonstration
v1.1.1 5/4/2012 Updated register names for ADIS16448/ADIS16485 to match datasheet names
Data Capture: changed “Cancel” button to “Stop”
v1.1.0 4/6/2012 Added support for the ADIS16485
Improvements to Waveform Recorder appearance
v1.0.1 3/27/2012 Addressed issue to enable correct register values in the Register Access menu
v1.0.0 3/24/2012 Initial Release

IMU EVALUATION SOFTWARE REVISION HISTORY

Click to display ⇲

Click to hide ⇱

REVISION RELEASE DATE SUMMARY OF UPDATES
v1.14.3 8/5/15 Adjust ADIS16210 registers to match recent datasheet updates
v1.14.2 TBD Internal update
v1.14.1 TBD Internal update
v1.14.0 3/2/15 Internal update
v1.13.0 Internal update
v1.12.0 Internal update
v1.11.1 4/9/14 Updated Magnetometer recorder in the Main Menu for consistency across the ADIS16405, ADIS16407, ADIS16448 and ADIS16488
v1.10.1 12/9/13 Address reported issue with SYS_E_FLAG register missing from ADIS16485 and ADIS16488 Register Access Menu
v1.10.0 11/1/13 Add support for the ADIS16137
Fix register access (GPIO_CTRL) in ADIS16209
v1.9.8 8/27/2013 Corrected a number of register definition issues on the ADIS16480
v1.9.7 8/21/2013 Corrected scale factors associated with GYRO_OUT/GYRO_OUT2 registers in the ADIS16133/5
v1.9.6 N/A Extended Precision Auto Null Wait time to 30 seconds on ADIS1636x/40x
NOTE: This version was not posted online, but these updates are in current versions
v1.9.5 N/A Corrected scale factors and offset factors associated with xTEMP_OUT on the ADIS16445
Corrected scale factors and offset factors associated with xTEMP_OUT and xMAGN_OUT registers in the ADIS16448
NOTE: This version was not posted online, but these updates are in current versions
v1.9.4 N/A Enabled support for using an external clock on the ADIS16405
NOTE: This version was not posted online, but these updates are in current versions
v1.9.3 3/18/2013 Added support for the ADIS16400 and ADIS16405
v1.9.2 2/18/2013 Changed the separation “de-limit” in the data captures file from a comma to a semicolon
v1.9.0 1/16/2013 Added support for the ADIS16209 and ADIS16210
Corrected scale factors associated with the xDELTVEL_xxx registers in the ADIS16480/5
v1.8.1 12/18/2013 Corrected a data capture error, which was observed in the ADIS16448, but could have impacted other products
v1.8.0 11/8/2013 Added support for external clock use
Added support for the ADIS16266
v1.7.0 10/1/12 Added support for the ADIS16360, ADIS16362, ADIS16364, ADIS16365, and ADIS16367
Corrected a scaling issue for those who use “Turkey” as their regional setting.
NOTE: Some sensitivity was still observed; some users in Turkey may need to change the regional setting to fully address.
v1.6.0 9/3/12 Added support for the ADIS16300 and ADIS16305
v1.5.0 8/22/12 Added support for the ADIS16445
v1.4.0 7/18/12 Added support for the ADIS1613, ADIS16135, ADIS16136 and ADIS16334
v1.3.0 N/A Internal updates
NOTE: This version was not posted online, but these updates are in current versions
v1.2.0 5/28/2012 Added support for the ADIS16480
Added 3-D viewer for ADIS16480 demonstration
v1.1.1 5/4/2012 Updated register names for ADIS16448/ADIS16485 to match datasheet names
Data Capture: changed “Cancel” button to “Stop”
v1.1.0 4/6/2012 Added support for the ADIS16485
Improvements to Waveform Recorder appearance
v1.0.1 3/27/2012 Addressed issue to enable correct register values in the Register Access menu
v1.0.0 3/24/2012 Initial Release

EXAMPLE EXERCISES

This section currently has no ADIS16362-specific content, but the ADIS16448 Evaluation on the EVAL-ADIS Wiki Site has some good examples to start with.

resources/eval/user-guides/inertial-mems/imu/adis1636x.txt · Last modified: 09 Jan 2021 00:39 by Robin Getz