This is an old revision of the document!
The EVAL-ADIS2 is a PC-based evaluation system that supports communication with most ADIS16xxx products, using the “breakout board” evaluation tools for each of these product. The following diagram illustrates the important connections between the device-under-test (DUT, ADIS16xxx) and a PC, when using the EVAL-ADIS2.
The following picture identifies the key features associated with this evaluation system. Click on the image to access a larger view.
For a complete listing of products that the EVAL-ADIS2 supports, please see the Tool Cross Reference listing in this Wiki Guide.
- EVAL-ADIS2 Evaluation Board
- Mini USB Cable, 6ft
- 16-pin IDC cable, 1.5“
- 16-pin IDC cable, 12”
- M2x0.4mm machine screw/hardware kit
NOTE: The EVAL-ADIS2 kit does not include the device-under-test (DUT) or breakout board. Those accessories need to be purchased separately. The Tool Cross Reference contains a list of model numbers (product and breakout board) that the EVAL-ADIS2 support.
- Microsoft Windows
- ADI SDP USB Driver
-.NET Framework 3.5
The following sequence of steps provides the quickest and most reliable process for setting up your EVAL-ADIS2 for operation on a PC.
JP1 provides three DUT power supply options: +3.3V, +5V and Ext (external supply).
Use the following table to identify the correct JP1 setting for the DUT:
JP1 = +3.3V | JP1 = +5V |
---|---|
ADIS16201, ADIS16203, ADIS16209, ADIS16210, ADIS16223, ADIS16227, ADIS16228, ADIS16375, ADIS16445, ADIS16448, ADIS16460, ADIS16465, ADIS16467, ADIS16470, ADIS16475, ADIS16477, ADIS16480, ADIS16485, ADIS16488A, ADIS16490, ADIS16495, ADIS16497 | ADIS16133, ADIS16135, ADIS16136, ADIS16137, ADIS16260, ADIS16265, ADIS16266, ADIS16300, ADIS16305, ADIS16334, ADIS16360, ADIS16362, ADIS16365, ADIS16367, ADIS16400, ADIS16405, ADIS16407 |
External Supply Option
In order to use external supply option, remove the header from JP1 and solder the middle post to the hole that has the EXT label on the EVAL-ADIS2. The next revision of this board will move this hole so that this option will be available using the same header that connects to the +3.3V and +5V settings on JP1.
Then, connect the external supply to J3, using the following diagram to illustrate the correct connections:
All ADIS16xxx (DUT) devices connect to the EVAL-ADIS2 through a breakout board. There are two different types of breakout boards: Model-specific and Generic. Model-specific breakout boards typically support products that require solder-reflow attachment, while Generic breakout boards typically support products that use some form of “press-in” connectors. So, the Model-specific breakout boards typically come have their DUT already installed onto the board, while the Generic breakout boards do not include the DUT (they have to be purchased separately).
The following table provides a summary of the most appropriate breakout board for each ADIS16xxx device, which uses a Generic breakout board to connect with the EVAL-ADIS2. TIP: Hover the mouse pointer over the breakout board (heading row in the table), right click on it, then click on Open in new tab to open useful setup instructions for that breakout board, in a new tab.
ADIS16IMU1/PCBZ | ADIS16IMU2/PCBZ | ADIS16IMU2/PCBZ ADIS1644X/FLEX | ADIS16IMU4/PCBZ | ADIS16ACL1/PCBZ | ADIS16ACL2/PCBZ |
---|---|---|---|---|---|
ADIS16133 ADIS16135 ADIS16136 ADIS16137 ADIS16375 ADIS16480 ADIS16485 ADIS16488A ADIS16490 ADIS16495 ADIS16497 | ADIS16360 ADIS16362 ADIS16364 ADIS16365 ADIS16367 ADIS16400 ADIS16405 ADIS16407 | ADIS16334 ADIS16445 ADIS16448 | ADIS16460 ADIS16465 ADIS16467 | ADIS16210 ADIS16228 | ADIS16223 ADIS16227 |
The J1 connector on the EVAL-ADIS2 supports remote connection to compatible breakout boards, using one of two IDC cables, which come with the EVAL-ADIS2 kit.
NOTE: The supporting connector (J1) on the ADIS1620x/PCBZ and ADIS1626x/PCBZ breakout boards only has 12-pins. In these cases, make sure that pin 1 (J1 on the ADIS1620x/PCBZ or ADIS1626x/PCBZ) connects to pin 1 on J1 of the EVAL-ADIS2.
Click here for more information on these special cases.
Download the USB driver for the EVAL-ADIS2 and store it in a convenient, temporary folder on the Test PC. Then, double click on this file. Answer all of the questions presented by the installation routine.
Click here to download the latest USB driver for the EVAL-ADIS2
After downloading the EVAL-ADIS USB Driver file, extract the SDPDrivers.exe file from the zip file, into a convenient location and then double click on it to start the process. When the setup wizard opens, click on Next to start the installation process
Click on Next to accept the default driver location.
The process will involve at least two progress bars that look like the following:
If you encounter this type of message during the process, click on Install to continue with the installation.
Once the installation has completed, click on Finish to complete the process.
Download the DUT's evaluation software package, but clicking on its heading in the following table. Store the file in a convenient location on the test PC and extract its executable file.
IMU Evaluation Software | Vibration Evaluation Software | ADIS16223 Vibration Evaluation Software |
---|---|---|
ADIS16133, ADIS16135, ADIS16136, ADIS16137, ADIS16201, ADIS16203, ADIS16260, ADIS16265, ADIS16266, ADIS16334, ADIS16360, ADIS16362, ADIS16364, ADIS16365, ADIS16367, ADIS16375, ADIS16400, ADIS16405, ADIS16407, ADIS16445, ADIS16448, ADIS16460, ADIS16465, ADIS16467, ADIS16470, ADIS16475, ADIS16477, ADIS16480, ADIS16485, ADIS16488A, ADIS16490, ADIS16495, ADIS16497 | ADIS16227, ADIS16228 | ADIS16223 |
Use a Mini USB cable to connect J2 (Mini USB connector) to a USB port on the PC. LED2 will light up very quickly and LED1 will take as long as 10 seconds to illuminate.
Double click on the executable file to launch the application software.
IMU Evaluation Software
Please visit the IMU Evaluation Software Wiki Guide to get some basic operational instructions.
Coming soon: Update to include latest version
Vibration Evaluation Software
Please visit the Vibration Evaluation Software Wiki Guide to get some basic operational instructions.
Coming soon: Update to include latest version
Coming soon: Product-specific tutorials, tips and tricks
The following table provides a list of products that the EVAL-ADIS2 supports, along with the appropriate breakout board, JP1 setting and software package for each of these products.
MODEL NUMBER | BREAKOUT BOARD | JP1 SETTING | SOFTWARE PACKAGE |
---|---|---|---|
ADIS16133BMLZ | ADIS16IMU1/PCBZ | +5V | IMU Evaluation Software |
ADIS16135BMLZ | ADIS16IMU1/PCBZ | +5V | IMU Evaluation Software |
ADIS16136BMLZ | ADIS16IMU1/PCBZ | +5V | IMU Evaluation Software |
ADIS16137BMLZ | ADIS16IMU1/PCBZ | +5V | IMU Evaluation Software |
ADIS16201CCCZ | ADIS16201/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16203CCCZ | ADIS16203/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16209CCCZ | ADIS16209/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16210BMLZ | ADIS16ACL1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16223CMLZ | ADIS16ACL2/PCBZ | +3.3V | ADIS16223 Vibration Evaluation Program |
ADIS16227CMLZ | ADIS16ACL2/PCBZ | +3.3V | Vibration Evaluation Program |
ADIS16228BMLZ | ADIS16ACL1/PCBZ | +3.3V | Vibration Evaluation Program |
ADIS16265BCCZ | ADIS16265/PCBZ | +5V | IMU Evaluation Software |
ADIS16334BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS1644X/FLEX | |||
ADIS16362BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16364BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16365BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16367BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16375BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16405BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16407BMLZ | ADIS16IMU2/PCBZ | +5V | IMU Evaluation Software |
ADIS16445BMLZ | ADIS16IMU2/PCBZ | +3.3V | IMU Evaluation Software |
ADIS1644X/FLEX | |||
ADIS16448BMLZ | ADIS16IMU2/PCBZ | +3.3V | IMU Evaluation Software |
ADIS1644X/FLEX | |||
ADIS16460AMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16465-1BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16465-2BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16465-3BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16467-1BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16467-2BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16467-3BMLZ | ADIS16IMU4/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16470AMLZ | ADIS16470/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16475-1BMLZ | ADIS16475-1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16475-2BMLZ | ADIS16475-2/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16475-3BMLZ | ADIS16475-3/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16477-1BMLZ | ADIS16477-1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16477-2BMLZ | ADIS16477-2/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16477-3BMLZ | ADIS16477-3/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16480BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16485BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16488BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16488CMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16490BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16495-1BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16495-2BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16495-3BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16497-1BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16497-2BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
ADIS16497-3BMLZ | ADIS16IMU1/PCBZ | +3.3V | IMU Evaluation Software |
Here is a temporary drawing, which shows the outer dimensions and the mounting hole locations. The nominal mounting hole diameter is 3.175mm.
Here are the pin assignments for J1, which is the connector that will interface with all of the ADIS16xxx breakout boards.
The EVAL-ADIS2 is compatible with most PCs that run Windows operating systems.
No official support Limited, please feel free to try these examples out.