Wiki

This version (13 Dec 2016 16:04) was approved by NevadaMark.The Previously approved version (10 Dec 2016 00:52) is available.Diff

ADIS16ACL2/PCB WIKI GUIDE

OVERVIEW

The ADIS16ACL2/PCBZ is the breakout board for the ADIS16223 and ADIS16227 vibration sensing solutions. This breakout board function helps connect these two products to the EVAL-ADIS2 evaluation system. It also helps connect these products to existing embedded processor platforms.

ORDERING

To order this breakout board, please visit the ADIS16ACL2/PCBZ's web page

ADIS16223/ADIS16227 Connection

Press the ADIS16223/7 connector onto J2 (14-pin socket).

EVAL-ADIS2 Connection

The EVAL-ADIS2 provides PC-based evaluation support for the ADIS16223 and ADIS16227. J1 on the EVAL-ADIS2Z and the ADIS16ACL2/PCBZ use the same pin assignments, so connecting them requires a 16-pin ribbon cable.

Electrical Schematic

Outer Dimensions

Mounting Holes

resources/eval/user-guides/inertial-mems/imu/adis16acl2-pcb.txt · Last modified: 13 Dec 2016 16:04 by NevadaMark

  沪ICP备09046653号