This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-aducm360-user-guide:installing_aducm36x_software_pack [24 Feb 2022 16:07] – Completed Raquel Grau | resources:eval:user-guides:eval-aducm360-user-guide:installing_aducm36x_software_pack [25 Feb 2022 13:08] (current) – Added IAR installation Raquel Grau | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Installing ADuCM36x Software Pack ====== | ====== Installing ADuCM36x Software Pack ====== | ||
- | The ADuCM36x Software Pack includes the C libraries to develop software for the ADuCM36x family with Keil μVision 5, as well as example code to help develop applications. The Software pack can be installed manually, downloading it from the [[https:// | + | The ADuCM36x Software Pack includes the C libraries to develop software for the ADuCM36x family with Keil μVision5 or IAR Embedded Workbench for ARM, as well as example code to help develop applications. |
- | ===== Manual | + | The Software Pack for Keil μVision5 can be installed manually, downloading it from the [[https:// |
+ | |||
+ | The Software Pack for IAR Embedded Workbench can be installed from the IAR application. | ||
+ | |||
+ | ===== Installation | ||
+ | |||
+ | ==== Manual Installation | ||
- Download Analog Devices ADuCM36x Device Support and Examples from [[https:// | - Download Analog Devices ADuCM36x Device Support and Examples from [[https:// | ||
- Install the ADuCM36x Pack in the default directory | - Install the ADuCM36x Pack in the default directory | ||
Line 10: | Line 16: | ||
</ | </ | ||
- | ===== Installation Through Keil μVision 5 ===== | + | ==== Installation Through Keil μVision5 |
- | - Open Keil μVision 5 | + | - Open Keil μVision5 |
- Open Pack Installer (See Figure 2) | - Open Pack Installer (See Figure 2) | ||
- | - Search for 'aducm' | + | - Search for **aducm** in the Search bar |
- | - In the Device list on the left-hand side, select | + | - In the Device list on the left-hand side, select |
- | - In the Packs tab on the right-hand side, expand | + | - In the Packs tab on the right-hand side, expand |
- | - Click 'Install' | + | - Click **Install** in **AnalogDevices:: |
- Accept the License Agreement | - Accept the License Agreement | ||
Line 26: | Line 32: | ||
}}<WRAP centeralign> | }}<WRAP centeralign> | ||
Figure 3. Installing the ADuCM36x Software Pack Trough the Pack Installer | Figure 3. Installing the ADuCM36x Software Pack Trough the Pack Installer | ||
+ | </ | ||
+ | |||
+ | ===== Installation for IAR Embedded Workbench ===== | ||
+ | - Open IAR Embedded Workbench. This will open IAR Embedded Workbench CMSIS Manager. | ||
+ | - In **Devices** -> **Search Device** Search for **aducm** and select **ADuCM36x Series** (Figure 4) | ||
+ | - With the device selected, go to **Packs** -> Device Specific** and install the pack **AnalogDevices.ADuCM36x_DFP** (Figure 5). | ||
+ | - Accept the license agreement. | ||
+ | |||
+ | {{ : | ||
+ | Figure 4. IAR CMSIS Manager. Selecting the ADuCM36x Series Device | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | Figure 3. Installing the ADuCM36x Software Pack | ||
</ | </ |