The ADuCM36x Software Pack includes the C libraries to develop software for the ADuCM36x family with Keil μVision5 or IAR Embedded Workbench for ARM, as well as example code to help develop applications.
The Software Pack for Keil μVision5 can be installed manually, downloading it from the Keil MDK5 Software Packs website, or it can be installed through the Pack Installer inside Keil μVision5.
The Software Pack for IAR Embedded Workbench can be installed from the IAR application.
Figure 1. Manual installation of ADuCM36x Software Pack
Figure 2. Opening Pack Installer
Figure 3. Installing the ADuCM36x Software Pack Trough the Pack Installer
Figure 4. IAR CMSIS Manager. Selecting the ADuCM36x Series Device
Figure 3. Installing the ADuCM36x Software Pack