Sensor software pack contains sensor software drivers and source code. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the EVAL-ADICUP3029 development platform. This software layer is the highest layer of abstraction from the microprocessor, and because of this can be useful to jump start code development for your application using any microprocessor. For example, if you are using the ADXL362, the Sensor software pack contains drivers and code snippets on the application level, so that can be transported to other microprocessor, with confidence that Analog Devices provided the application framework pieces. When combined with the ADuCM302x and ADICUP3029 software packs there are many great Internet of Things(IoT) applications and demos that can be replicated using the ADICUP3029 development platform.
ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and ADICUP3029 Board Support Package 1.1.0.
For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the ADICUP3029 platform.
The software pack can be downloaded in several ways.
Download the Sensor Software Pack to your computer.
Link to Github Repository for Cloning or Viewing.
End of Document