Wiki

This version is outdated by a newer approved version.DiffThis version (18 Aug 2017 17:20) was approved by Brandon Bushey.The Previously approved version (02 Jun 2017 22:53) is available.Diff

This is an old revision of the document!


Sensors Software Pack

General Description/Overview

Sensor software pack contains sensor software drivers and source code. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the EVAL-ADICUP3029 development platform. This software layer is the highest layer of abstraction from the microprocessor, and because of this can be useful to jump start code development for your application using any microprocessor. For example, if you are using the ADXL362, the Sensor software pack contains drivers and code snippets on the application level, so that can be transported to other microprocessor, with confidence that Analog Devices provided the application framework pieces. When combined with the ADuCM302x and ADICUP3029 software packs there are many great Internet of Things(IoT) applications and demos that can be replicated using the ADICUP3029 development platform.

ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and ADICUP3029 Board Support Package 1.1.0.

For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide.

You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the ADICUP3029 platform.

Downloading the Sensor Software Pack

The software pack can be downloaded in several ways.

  1. Downloaded via the tools program
    • It is recommended to download the Sensor software pack through from the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the Sensor software pack through CrossCore Embedded Studio please see our CrossCore Embedded Studio Quickstart User Guide.
  2. Downloaded to local directory
    • However if you do decide to download the Sensor software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.
  3. Cloning the ADICUP3029 Github Repository
    • Cloning a public facing Git repository can be done through the CrossCore Embedded Studios tools or directly from the Github website (which will store it to a local directory on your computer.) The same general rules apply from above, where importing the example from Github through the tools package is recommended, over downloading the zip file and storing it to a directory of your choice.

Download the Sensor Software Pack to your computer.

Sensors Software Pack 1.1.0


Link to Github Repository for Cloning or Viewing.

EVAL-ADICUP3029 Sensor Software Pack Github Repository

End of Document

resources/eval/user-guides/eval-adicup3029/software/sensors.1503069646.txt.gz · Last modified: 18 Aug 2017 17:20 by Brandon Bushey