BLE Software Pack
This CMSIS pack and its contents are DEPRECATED and no longer supported. Please do not use this moving forward
General Description/Overview
BLE software pack contains source code written to interface the ADuCM3029 with the EM9304 radio.(Found on the EVAL-ADICUP3029) This software package acts as a library that can be used with any platform containing the ADuCM3029 and the EM9304.
To use the ADI_BLESoftware Pack with the ADICUP3029, you will also require the following software, tools, CMSIS Packs:
CrossCore Embedded Studio
ADuCM302x Device Family Pack
ADICUP3029 Board Support Package
For detailed information regarding the BLE software pack, please see our complete BLE software user guide.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications using the Bluetooth for the ADICUP3029 platform.
Downloading the BLE Software Pack
The software pack can be downloaded in several ways.
Downloaded via the tools program
It is
recommended to download the BLE software pack through from within the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the BLE software pack through CrossCore Embedded Studio please see our
CrossCore Embedded Studio Quickstart User Guide.
Downloaded to local directory
However if you do decide to download the BLE software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.
End of Document