Wiki

This version is outdated by a newer approved version.DiffThis version (30 Jul 2019 20:09) was approved by Brandon Bushey.The Previously approved version (30 Jul 2019 20:00) is available.Diff

This is an old revision of the document!


BLE Software Pack

General Description/Overview

BLE software pack contains source code written to interface the ADuCM3029 with the EM9304 radio.(Found on the EVAL-ADICUP3029) This software package acts as a library that can be used with any platform containing the ADuCM3029 and the EM9304.

To use the ADI_BLESoftware Pack with the ADICUP3029, you will also require the following software, tools, CMSIS Packs:

  • CrossCore Embedded Studio
  • ADuCM302x Device Family Pack
  • ADICUP3029 Board Support Package

For detailed information regarding the BLE software pack, please see our complete BLE software user guide.

You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications using the Bluetooth for the ADICUP3029 platform.

Downloading the BLE Software Pack

The software pack can be downloaded in several ways.

  1. Downloaded via the tools program
    • It is recommended to download the BLE software pack through from within the tools program you are using. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the BLE software pack through CrossCore Embedded Studio please see our CrossCore Embedded Studio Quickstart User Guide.
  2. Downloaded to local directory
    • However if you do decide to download the BLE software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/projects.

Download the BLE Software Pack to your computer.

ADI_BLESoftware Pack 1.0.1

End of Document

resources/eval/user-guides/eval-adicup3029/software/ble_sw.1564510156.txt.gz · Last modified: 30 Jul 2019 20:09 by Brandon Bushey