This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup3029:smart_app:ios_app [22 May 2017 09:21] – [How to Run ADIoTNode] Pranit Jadhav | resources:eval:user-guides:eval-adicup3029:smart_app:ios_app [30 Jul 2019 20:59] (current) – updating to IoTNode 2.0 Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== iOS Smart Device App ====== | + | ====== iOS Smart App Overview ====== |
- | ====== iOS App Overview ====== | + | |
- | **ADIoTNode** is iOS Smart Device App developed by **Analog Devices Inc.** to showcase example | + | **IoTNode** is iOS Smart Device App developed by **Analog Devices Inc.** to showcase example |
===== iOS Device Minimum Requirement ===== | ===== iOS Device Minimum Requirement ===== | ||
Line 10: | Line 9: | ||
* Bluetooth Version: v4 or higher | * Bluetooth Version: v4 or higher | ||
- | ====== Using the Pre-Build App ====== | + | ===== How to Download & Install |
- | ===== How to Download & Install | + | Follow below instructions to download Analog Devices |
- | Follow below instructions to download Analog Devices | + | |
- Go to App Store on your iOS Device. | - Go to App Store on your iOS Device. | ||
- | - Search **ADIoTNode**. Make sure you select 1.0 version. | + | - Search **IoTNode**. |
- Tap " | - Tap " | ||
Wait until installation is successful. | Wait until installation is successful. | ||
- | ===== How to Run ADIoTNode ===== | + | <WRAP round 40% download> |
- | Follow below instructions to run the App. | + | Direct link to [[https://appsto.re/ |
- | - Turn on device Bluetooth by navigating to Settings -> Bluetooth -> Turn ON Slider. | + | </ |
- | - iOS homescreen navigate | + | |
- | - Below is **ADIoTNode** app homesceen. {{ : | + | |
- | - Now tap "Tap To Connect" | + | |
- | - Tap on " | + | |
+ | ===== How to use IoTNode ===== | ||
+ | |||
+ | Follow below instructions to run the App. | ||
+ | - Turn on device Bluetooth by navigating to Settings -> Bluetooth -> Turn Slider **ON**. | ||
+ | - On the iOS homescreen navigate to **IoTNode** and tap to open. {{ : | ||
+ | - Once open, the app should automatically find Bluetooth devices within range, so you'll want to find and open the project you are working on. | ||
+ | - Once connected, the app will provide you an option for which sensor(s) you are connected to that Bluetooth device. | ||
+ | - It's usually only a single sensor, so make sure it's " | ||
+ | - You are now connected, and data should start to display on the app.{{ : | ||
- | ====== Obtain the Source Code for the App ====== | + | ===== Interfacing Data to IoTNode |
+ | The **IoTNode** app supports an easy to interface registration, | ||
+ | * [[resources: | ||