This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:circuits-from-the-lab:cn0364 [03 Jan 2021 21:55] – fix links Robin Getz | resources:eval:user-guides:circuits-from-the-lab:cn0364 [06 Jan 2021 08:28] (current) – Fixed bad link for EVAL-CN0364-SDPZ and removed reference for EVAL-SDP-CB1Z Ioana Chelaru | ||
---|---|---|---|
Line 8: | Line 8: | ||
This user guide will discuss how to use the [[adi> | This user guide will discuss how to use the [[adi> | ||
- | A complete design support package for the [[adi> | + | A complete design support package for the [[adi>CN0364|EVAL-CN0364-SDPZ]] evaluation board containing schematics, layouts (native and Gerber), and bill-of-materials can be found at: [[adi> |
{{ : | {{ : | ||
Line 15: | Line 15: | ||
===== Required Equipment ===== | ===== Required Equipment ===== | ||
- | * [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ Evaluation Board]] | + | * [[adi> |
- | * [[adi>EVAL-SDP-CB1Z|EVAL-SDP-CB1Z]] | + | * EVAL-SDP-CB1Z Controller Board (**SDP-B Board**) |
* DC Power Supply (+12V to +24V) | * DC Power Supply (+12V to +24V) | ||
* Precision voltage and current source (for input) | * Precision voltage and current source (for input) | ||
Line 31: | Line 31: | ||
===== General Setup ===== | ===== General Setup ===== | ||
{{ : | {{ : | ||
- | * The [[adi>EVAL-CN0364-SDPZ|EVAL-CN0364-SDPZ]] **(CN-0364 Board)** connects to the [[adi> | + | * The [[adi> |
* The [[adi> | * The [[adi> | ||
* Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC | * Header **P10** is a PMOD compatible SPI header - allows for communication to the ADC |