The AD9695 is a dual 14-bit, 1300/625MSPS analog-to-digital converter (ADC) featuring an on-chip buffer and a sample-and-hold circuit designed for low power, small size, and ease of use. The dual ADC cores feature a multistage, differential pipelined architecture with integrated output error correction logic. Each ADC features wide bandwidth inputs supporting a variety of user-selectable input ranges.
The AD9695-FMC reference design is a processor based (e.g. Microblaze) embedded system. The design consists of a receive chain that transports the captured samples from the ADC to the system memory (DDR).
All cores from the receive chain are programmable through an AXI-Lite interface.
Only the channels presented in the clocking selection are relevant. For the rest, you can either disable them or just put a divided frequency of the source clock.
The data path and clock domains are depicted on the below diagram:
The design has one JESD receive chain with 4 lanes at rate of 13Gbps. The JESD receive chain consists of a physical layer represented by an XCVR module, a link layer represented by an RX JESD LINK module and transport layer represented by a RX JESD TPL module. The link operates in Subclass 1.
The link is set for full bandwidth mode and operate with the following parameters:
Deframer paramaters: L=4, M=2, F=1, S=1, N’=16
SYSREF - 5.078125 MHZ
REFCLK – 325MHz (Lane Rate/40)
DEVICECLK -325 MHz
ADCCLK – 1300MHz
JESD204B Lane Rate – 13Gbps
The transport layer component presents on its output 128 bits at once on every clock cycle, representing 4 samples per converter. The two receive chains are merged together and transferred to the DDR with a single DMA.
ADI does not distribute the bit/elf files of these projects so they must be built from the sources available here. To get the source you must clone the HDL repository. Then go to the /projects/ad9695_fmc/zcu102 location and run the make command by typing in your command prompt:
Linux/Cygwin
user@analog:~$ cd hdl/projects/ad9695_fmc/zcu102 user@analog:~/hdl/projects/ad9695_fmc/zcu102$ make
A more comprehensive build guide can be found in the HDL User Guide.
AD9695 connected to ZCU102 on FMC HPC1
ZCU102 | SYNCRONA |
---|---|
J79 | CH9_P |
J80 | CH9_N |
ADC9695 EVAL | SYNCRONA |
---|---|
J202 | CH10_P |
J200 | CH13 |
P202 | CH14 |
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.