This is an old revision of the document!
The AD9656 is a quad 16-bit, 125MSPS analog-to-digital converter (ADC) with an on-chip sample and hold circuit designed for low cost, low power, small size, and ease of use. The AD9656EBZ board is build around the AD9656 chip and it pairs with a carrier board through a FMC connector. The ADC chip uses the JESD204B protocol to transfer the data to the carrier board. The SPI protocol is used by the carrier board to configure the parameters from the register file of the ADC and the two clock chips.
Until now our recommended plaform is the Zynq based system:
The reference design is a processor based ARM embedded system. A functional block diagram of the system is given below for the Xilinx FPGAs. The cores are programmable through an AXI-lite interface. The data path consists of a DMA interface for the receive path.
The digital interface consists of 4 receive lanes running at 2.5Gbps. The transceivers then interfaces to the cores at 128bits@62.5MHz. The data is received based on the configuration (programmable) from separate receive chains.
The ADC data is sent to the DDR via DMA. The core also supports PN monitoring at the sample level. This is different from the JESD204B specific PN sequence.
The device control and monitor signals are interfaced to a GPIO module. The SPI signals are controlled by a separate AXI based SPI core.
ADI does not distribute the bit/elf files of these projects so they must be built from the sources available here. To get the source you must clone the HDL repository. Then go to the /projects/ad9656_fmc/zcu102 location and run the make command by typing in your command prompt:
Linux
dhotolea@analog:~$ cd hdl/projects/ad9656_fmc/zcu102 dhotolea@analog:~/hdl/projects/ad9656_fmc/zcu102$ make
The Makefile script will use the two TCL files, the constraints file and the system top level Verilog file available in the current folder along with the script from the /projects/ad9656_fmc/common folder and will generate a Vivado project. The constraints file contains only the constraints that are specific for the AD9656 project. The rest of the constraints that are embedded in this design are available in the folder /projects/common/zcu102.
After the Makefile finishes the Hardware Description File system_top.hdf file should be generated in the /projects/ad9656_fmc/zcu102/ad9656_fmc_zcu102.sdk folder.
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD3552REVB | ad3552r_evb | zed | ad3552r_evb_zed | axi_ad3552r |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD40XXFMC | ad40xx_fmc | zed | ad40xx_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom | ||||
util_i2c_mixer |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD4110-1 | ad4110 | zed | ad4110_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD4134 | ad4134_fmc | zed | ad4134_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD4630FMC | ad4630_fmc | zed | ad4630_fmc_zed | ad463x_data_capture |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_axis_reorder | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD469XFMC | ad469x_fmc | zed | ad469x_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD4858FMCZ | ad4858_fmcz | zed | ad4858_fmcz_zed | axi_ad4858 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD5766SDZ | ad5758_sdz | zed | ad5758_sdz_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD5766SDZ | ad5766_sdz | zed | ad5766_sdz_zed | axi_ad5766 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD6676EBZ | ad6676evb | vc707 | ad6676evb_vc707 | axi_adxcvr |
zc706 | ad6676evb_zc706 | axi_clkgen | ||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD7134FMC | ad7134_fmc | zed | ad7134_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD79XASDZ | ad719x_asdz | coraz7s | ad719x_asdz_coraz7s | axi_sysid |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD738xFMC | ad738x_fmc | zed | ad738x_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD7405FMC | ad7405_fmc | zed | ad7405_fmc_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_dec256sinc24b |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD7606 | ad7606x_fmc | zed | ad7606x_fmc_zed | axi_ad7606x |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD7616SDZ | ad7616_sdz | zed | ad7616_sdz_zed | axi_ad7616 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD77681EBZ | ad77681evb | zed | ad77681evb_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD7768EBZ | ad7768evb | zed | ad7768evb_zed | axi_ad7768 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD777XARDZ | ad777x_ardz | de10nano | NA | axi_ad777x |
zed | ad777x_ardz_zed | axi_clkgen | ||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9081FMCAEBZ-X-BAND | ad9081_fmca_ebz_x_band | zcu102 | ad9081_fmca_ebz_x_band_zcu102 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_sysid | ||||
axi_tdd | ||||
data_offload | ||||
jesd204_rx | ||||
jesd204_tx | ||||
jesd204_versal_gt_adapter_rx | ||||
jesd204_versal_gt_adapter_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_axis_fifo | ||||
util_cdc | ||||
util_cpack2 | ||||
util_dacfifo | ||||
util_do_ram | ||||
util_hbm |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9083VB | ad9083_evb | a10soc | NA | ad_ip_jesd204_tpl_adc |
zcu102 | ad9083_evb_zcu102 | axi_adxcvr | ||
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9083VNA | ad9083_vna | zcu102 | ad9083_vna_zcu102 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9208DUAL | ad9208_dual_ebz | vcu118 | ad9208_dual_ebz_vcu118 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9209 | ad9209_fmca_ebz | vck190 | ad9209_fmca_ebz_vck190 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_sysid | ||||
axi_tdd | ||||
data_offload | ||||
jesd204_rx | ||||
jesd204_tx | ||||
jesd204_versal_gt_adapter_rx | ||||
jesd204_versal_gt_adapter_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_axis_fifo | ||||
util_cdc | ||||
util_cpack2 | ||||
util_dacfifo | ||||
util_do_ram | ||||
util_hbm |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9213DUAL | ad9213_dual_ebz | s10soc | NA | ad_ip_jesd204_tpl_adc |
axi_dmac | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9213EVB | ad9213_evb | vcu118 | ad9213_evb_vcu118 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adcfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9265-FMC-125EBZ | ad9265_fmc | zc706 | ad9265_fmc_zc706 | axi_ad9265 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_spdif_tx | ||||
axi_sysid |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9434-FMC-500EBZ | ad9434_fmc | zc706 | ad9434_fmc_zc706 | axi_ad9434 |
zed | ad9434_fmc_zed | axi_clkgen | ||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9467-FMC-250EBZ | ad9467_fmc | kc705 | ad9467_fmc_kc705 | axi_ad9467 |
zed | ad9467_fmc_zed | axi_clkgen | ||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9656FMC | ad9656_fmc | zcu102 | ad9656_fmc_zcu102 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9695FMC | ad9695_fmc | zcu102 | ad9695_fmc_zcu102 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9739A-FMC-EBZ | ad9739a_fmc | zc706 | ad9739a_fmc_zc706 | axi_ad9739a |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_spdif_tx | ||||
axi_sysid |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD9783-EBZ | ad9783_ebz | zcu102 | ad9783_ebz_zcu102 | axi_ad9783 |
axi_dmac | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADFMCLIDAR1EBZ | ad_fmclidar1_ebz | a10soc | NA | ad_ip_jesd204_tpl_adc |
zc706 | ad_fmclidar1_ebz_zc706 | axi_adxcvr | ||
zcu102 | ad_fmclidar1_ebz_zcu102 | axi_clkgen | ||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_laser_driver | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADQUADMXFE1EBZ | ad_quadmxfe1_ebz | vcu118 | ad_quadmxfe1_ebz_vcu118 | axi_adxcvr |
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_cpack2 | ||||
util_dacfifo | ||||
util_pad |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADAQ7980-SDZ | adaq7980_sdz | zed | adaq7980_sdz_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADAQ8092-FMC | adaq8092_fmc | zed | adaq8092_fmc_zed | axi_adaq8092 |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-ADRV9001 | adrv9001 | a10soc | NA | axi_adrv9001 |
zc706 | adrv9001_zc706 | axi_clkgen | ||
zcu102 | adrv9001_zcu102 | axi_dmac | ||
zed | adrv9001_zed | axi_hdmi_tx | ||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 | ||||
util_i2c_mixer | ||||
util_rfifo | ||||
util_upack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-ADRV9008/9 | adrv9009 | a10soc | NA | ad_ip_jesd204_tpl_adc |
s10soc | NA | ad_ip_jesd204_tpl_dac | ||
zc706 | adrv9009_zc706 | axi_adxcvr | ||
zcu102 | adrv9009_zcu102 | axi_clkgen | ||
axi_dacfifo | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adxcvr | ||||
util_cpack2 | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-ADRV9026 | adrv9026 | a10soc | adrv9026_a10soc | ad_ip_jesd204_tpl_adc |
zcu102 | adrv9026_zcu102 | ad_ip_jesd204_tpl_dac | ||
axi_adxcvr | ||||
util_adxcvr | ||||
util_dacfifo | ||||
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
jesd204_rx | ||||
jesd204_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 | ||||
util_upack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADRV9371 | adrv9371x | a10soc | NA | ad_ip_jesd204_tpl_adc |
kcu105 | adrv9371x_kcu105 | ad_ip_jesd204_tpl_dac | ||
zc706 | adrv9371x_zc706 | axi_adxcvr | ||
zcu102 | adrv9371x_zcu102 | axi_clkgen | ||
axi_dacfifo | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adxcvr | ||||
util_cpack2 | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ADV7511 | adv7511 | zc702 | adv7511_zc702 | axi_clkgen |
zc706 | adv7511_zc706 | axi_dmac | ||
zed | adv7511_zed | axi_hdmi_tx | ||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
ARRadio | arradio | c5soc | NA | axi_ad9361 |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 | ||||
util_rfifo | ||||
util_upack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0363 | cn0363 | zed | cn0363_zed | axi_clkgen |
axi_dmac | ||||
axi_generic_adc | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
cn0363_dma_sequencer | ||||
cn0363_phase_data_sync | ||||
cordic_demod | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom | ||||
util_axis_resize | ||||
util_i2c_mixer |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0506 | cn0506 | a10soc | NA | axi_clkgen |
zc706 | cn0506_zc706 | axi_dmac | ||
zcu102 | cn0506_zcu102 | axi_hdmi_tx | ||
zed | cn0506_zed | axi_i2s_adi | ||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_i2c_mixer |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0540 | cn0540 | coraz7s | cn0540_coraz7s | axi_clkgen |
de10nano | NA | axi_dmac | ||
axi_hdmi_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0561 | cn0561 | coraz7s | cn0561_coraz7s | axi_clkgen |
de10nano | NA | axi_dmac | ||
zed | cn0561_zed | axi_hdmi_tx | ||
axi_i2s_adi | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0577 | cn0577 | zed | cn0577_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_ltc2387 | ||||
axi_pwm_gen | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
CN0579 | cn0579 | coraz7s | cn0579_coraz7s | axi_ad7768 |
de10nano | NA | axi_dmac | ||
axi_hdmi_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
EVAL-AD9135 | dac_fmc_ebz | a10soc | NA | ad_ip_jesd204_tpl_dac |
EVAL-AD9136 | vcu118 | dac_fmc_ebz_vcu118 | axi_adxcvr | |
EVAL-AD9144 | zc706 | dac_fmc_ebz_zc706 | axi_clkgen | |
EVAL-AD9152 | zcu102 | dac_fmc_ebz_zcu102 | axi_dmac | |
EVAL-AD9154 | axi_hdmi_tx | |||
EVAL-AD916x | axi_jesd204_tx | |||
EVAL-AD917x | axi_spdif_tx | |||
axi_sysid | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adxcvr | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
DC2677A | dc2677a | c5soc | NA | axi_dmac |
axi_hdmi_tx | ||||
axi_pwm_gen | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCADC2-EBZ | fmcadc2 | vc707 | fmcadc2_vc707 | axi_adcfifo |
AD-FMCADC3-EBZ | zc706 | fmcadc2_zc706 | axi_adxcvr | |
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adcfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCADC5-EBZ | fmcadc5 | vc707 | fmcadc5_vc707 | axi_ad9625 |
axi_adxcvr | ||||
axi_dmac | ||||
axi_fmcadc5_sync | ||||
axi_jesd204_rx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCDAQ2-EBZ | daq2 | a10soc | NA | ad_ip_jesd204_tpl_adc |
kc705 | daq2_kc705 | ad_ip_jesd204_tpl_dac | ||
kcu105 | daq2_kcu105 | axi_adxcvr | ||
zc706 | daq2_zc706 | axi_clkgen | ||
zcu102 | daq2_zcu102 | axi_dmac | ||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
data_offload | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_axis_fifo | ||||
util_cdc | ||||
util_cpack2 | ||||
util_do_ram | ||||
util_hbm |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCDAQ3-EBZ | daq3 | kcu105 | daq3_kcu105 | axi_adcfifo |
vcu118 | daq3_vcu118 | axi_adxcvr | ||
zc706 | daq3_zc706 | axi_clkgen | ||
zcu102 | daq3_zcu102 | axi_dmac | ||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adcfifo | ||||
util_adxcvr | ||||
util_cpack2 | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCJESDADC1-EBZ | fmcjesdadc1 | kc705 | fmcjesdadc1_kc705 | axi_adxcvr |
vc707 | fmcjesdadc1_vc707 | axi_clkgen | ||
zc706 | fmcjesdadc1_zc706 | axi_dmac | ||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
sysid_rom | ||||
util_adxcvr |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCOMMS11-EBZ | fmcomms11 | zc706 | fmcomms11_zc706 | axi_adcfifo |
axi_adxcvr | ||||
axi_clkgen | ||||
axi_dmac | ||||
axi_hdmi_tx | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adxcvr | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCOMMS2-EBZ | fmcomms2 | kc705 | fmcomms2_kc705 | axi_ad9361 |
AD-FMCOMMS3-EBZ | kcu105 | fmcomms2_kcu105 | axi_clkgen | |
AD-FMCOMMS4-EBZ | vc707 | fmcomms2_vc707 | axi_dmac | |
zc702 | fmcomms2_zc702 | axi_hdmi_tx | ||
zc706 | fmcomms2_zc706 | axi_i2s_adi | ||
zcu102 | fmcomms2_zcu102 | axi_spdif_tx | ||
zed | fmcomms2_zed | axi_sysid | ||
sysid_rom | ||||
util_clkdiv | ||||
util_cpack2 | ||||
util_i2c_mixer | ||||
util_rfifo | ||||
util_tdd_sync | ||||
util_upack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCOMMS5-EBZ | fmcomms5 | zc702 | fmcomms5_zc702 | axi_ad9361 |
zc706 | fmcomms5_zc706 | axi_clkgen | ||
zcu102 | fmcomms5_zcu102 | axi_dmac | ||
axi_hdmi_tx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom | ||||
util_clkdiv | ||||
util_cpack2 | ||||
util_rfifo | ||||
util_upack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AD-FMCOMMS8-EBZ | fmcomms8 | a10soc | NA | ad_ip_jesd204_tpl_adc |
zcu102 | fmcomms8_zcu102 | ad_ip_jesd204_tpl_dac | ||
axi_adxcvr | ||||
axi_dmac | ||||
axi_jesd204_rx | ||||
axi_jesd204_tx | ||||
axi_sysid | ||||
jesd204_rx | ||||
jesd204_tx | ||||
sysid_rom | ||||
util_adxcvr | ||||
util_cpack2 | ||||
util_dacfifo |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
AES-FMC-IMAGEON-G | imageon | zed | imageon_zed | axi_clkgen |
axi_dmac | ||||
axi_hdmi_rx | ||||
axi_hdmi_tx | ||||
axi_i2s_adi | ||||
axi_spdif_rx | ||||
axi_spdif_tx | ||||
axi_sysid | ||||
sysid_rom |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
JUPITER-SDR | jupiter_sdr | jupiter_sdr | jupiter_sdr_jupiter_sdr | axi_adrv9001 |
axi_dmac | ||||
axi_sysid | ||||
sysid_rom | ||||
util_cpack2 |
Hardware | Project | Carriers | Resource Utilization | Library Cores |
---|---|---|---|---|
PULSAR-ADC-PMDZ | pulsar_adc_pmdz | coraz7s | pulsar_adc_pmdz_coraz7s | axi_clkgen |
axi_dmac | ||||
axi_pwm_gen | ||||
axi_spi_engine | ||||
axi_sysid | ||||
spi_engine_execution | ||||
spi_engine_interconnect | ||||
spi_engine_offload |