This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [16 Sep 2021 15:23] – [Prepare SD card] Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [02 Nov 2021 09:14] – [Troubleshooting] Septimiu Vana | ||
---|---|---|---|
Line 31: | Line 31: | ||
<note important> | <note important> | ||
{{: | {{: | ||
+ | <note important> | ||
+ | {{: | ||
+ | <note important> | ||
==== Power off sequence ==== | ==== Power off sequence ==== | ||
Line 43: | Line 46: | ||
* The SD card is corrupted and this prevents the system from booting. Reflash the SD card or check generated devicetree or kernel image | * The SD card is corrupted and this prevents the system from booting. Reflash the SD card or check generated devicetree or kernel image | ||
+ | * The demo application hangs after closing the main window | ||
+ | * Due to some limitations the application always hangs if it is closed using the regular X button from the window top bar (title bar). To avoid this unpleasant hang, we've made available a second X button in the top right corner right above the title bar that can be used to safely close the demo application. We hope this to be a temporary workaround. | ||
---- | ---- | ||
===== Running the evaluation application ===== | ===== Running the evaluation application ===== | ||
- | [[https:// | + | [[https:// |
+ | |||
+ | Once Linux boots you'll see on the HDMI monitor the Linux desktop and on the top left corner a shortcut | ||
+ | |||
+ | {{: | ||
+ | |||
+ | When starting the application, | ||
+ | |||
+ | The evaluation application allows to do live streaming of depth and IR data as well as recording the depth and IR data and playing back from a file. The depth data is displayed as a color map ranging from warm to cold colors as the distance from the camera increases. A point in the middle of the depth image shows the distance in mm to the target. | ||
+ | |||
+ | There are 3 operating modes that determine the range of the system: | ||
+ | |||
+ | * Near - 25cm to 80cm | ||
+ | * Medium - 30cm to 3m | ||
+ | |||
+ | When in a certain operating mode the system will measure distances outside of the mode's range but those will not be accurate. The evaluation application also displays the temperature in deg C of the camera (AFE). | ||
+ | |||
+ | The framerate at which data is acquired from the system is constantly updated on the GUI. The camera board outputs data at 30 frames per second (fps), but due to USB connection limitations, | ||
{{navigation AD-FXTOF1-EBZ# | {{navigation AD-FXTOF1-EBZ# | ||