This is an old revision of the document!
Nvidia Jetson Nano User Guide
Setting up the system
Required hardware
Prepare SD card
Power on sequence
Plug the
SD card into the Nvidia Jetson
SD card slot
Connect the HDMI cable from the monitor to the Jetson HDMI connector
Connect the 25 pins flex cable between the camera and the interposer
Connect the 15 pins camera cable between the Jetson Nano and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides.
Connect a
USB mouse and keyboard to the Jetson
Connect the interposer to the power supply
connect the 5V power supply to the Jetson Nano. Once power is connected to the Jetson the system will boot the Linux
OS from the
SD card.
Password for “analog” user is “analog”. This user has sudo rights
Power off sequence
Troubleshooting
Linux does not boot
The
SD card is corrupted and this prevents the system from booting. Reflash the
SD card or check generated devicetree or kernel image
Running the evaluation application
This example demonstrates how to capture data from the TOF system on the Nvidia jetson and display it using OpenCV. Due to limitations in the Nvidia Jetson software infrastructure for MIPI virtual channels support, only one video stream is available at a time, depth or IR.