Wiki

This version (22 Sep 2021 14:26) was approved by Septimiu Vana.The Previously approved version (16 Sep 2021 15:23) is available.Diff

Nvidia Jetson Nano User Guide

Setting up the system

Required hardware

  • 5V power supply for Jetson. (Jetson board can be powered up from USB but external 4A 5V supply is recommended)
  • 5V power supply for the interposer.
  • To run the system in standalone mode, besides the accessories that are provided in the AD-FXTOF1-EBZ box you'll need an additional HDMI cable to connect to a monitor and a USB keyboard and mouse
  • Camera flex cable for connection between Jetson and AD-FXTOF1-EBZ

Prepare SD card

  • Download and flash on a SD card the latest image provided from the following link: aditof_sdk#ad-fxtof1-ebz
  • Download L4T BSP L4T BSP package (Tested release R32.3.1)
  • Extract kernel_src from BSP package
  • ADI ToF camera driver and devicetree should be taken from aditof_sdk
  • Copy paste and replace content of kernel_src folder from L4T BSP with the one downloaded from ADI ToF Repository
  • Build Kernel and devicetree blob following instructions from Building_the_Kernel_from_Source selecting “CONFIG_VIDEO_ADDI9036” and “CONFIG_EEPROM_AT24” using menuconfig
  • Copy generated kernel Image and devicetree to SD card

Power on sequence

  • Plug the SD card into the Nvidia Jetson SD card slot
  • Connect the HDMI cable from the monitor to the Jetson HDMI connector
  • Connect the 25 pins flex cable between the camera and the interposer
  • Connect the 15 pins camera cable between the Jetson Nano and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides.
  • Connect a USB mouse and keyboard to the Jetson
  • Connect the interposer to the power supply
  • connect the 5V power supply to the Jetson Nano. Once power is connected to the Jetson the system will boot the Linux OS from the SD card.
Password for “analog” user is “analog”. This user has sudo rights

One CSI connector board version

Two CSI connectors board version

Power off sequence

  • Open a terminal and type sudo poweroff. This will safely power off and ensure that the SD card is properly unmounted
  • remove the 5V supply from the Nvidia Jetson
  • remove the 5V supply from the interposer

Troubleshooting

  • Linux does not boot
    • The SD card is corrupted and this prevents the system from booting. Reflash the SD card or check generated devicetree or kernel image

Running the evaluation application

This example demonstrates how to capture data from the TOF system on the Nvidia jetson and display it using OpenCV. Due to limitations in the Nvidia Jetson software infrastructure for MIPI virtual channels support, only one video stream is available at a time, depth or IR.

Navigation - AD-FXTOF1-EBZ

resources/eval/user-guides/ad-fxtof1-ebz/ug_jetson.txt · Last modified: 22 Sep 2021 14:25 by Septimiu Vana