This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [20 Feb 2015 09:32] – created Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:14] – [Required Hardware] Andrei Cozma | ||
---|---|---|---|
Line 11: | Line 11: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * AD-FMCMOTCON2-EBZ - Controller board. | + | * AD-FMCMOTCON2-EBZ - Controller board |
- | * AD-DRVLV2-EBZ - Low voltage drive board. | + | * AD-DRVLV2-EBZ - Low voltage drive board |
- | * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional). | + | * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional) |
* [[http:// | * [[http:// | ||
- | * 24V 3A capable | + | * 12V - 48V capable |
|< 100% 100% >| | |< 100% 100% >| |