ADI FMC Motor Drive System v2 Introduction
The ADI FMC motor drive v2 solution consist of the following products
AD-FMCMOTCON2-EBZ - Controller board. Compatible with all Xilinx FPGA platforms with FMC LPC or HPC connectors.
AD-DRVLV2-EBZ - Low voltage drive board. Connects to the Controller board and has a power stage that can drive Brushed DC / BLDC / PMSM / Stepper motors up to 48V and 20A.
AD-DYNO2-EBZ - Dynamometer drive system. Acts as an electronically adjustable load with two BLDC motors connected in a dyno setup.
AD-FMCMOTCON2-EBZ | AD-DRVLV2-EBZ | AD-DYNO2-EBZ |
| | |
The Controller and the Drive boards are provided as a kit and cannot be purchased separately. They are both distributed under the AD-FMCMOTCON2-EBZ part number.
Purpose
Provide an efficient drive system for different types of electric motors
Address power and isolation challenges encountered in motor control applications
Provide accurate measurement of motor feedback signals
Achieve flexible control with FPGA/SoC interface
High speed industrial Ethernet interface
Added Value
Complete control solution showing how to integrate hardware for
Power
Isolation
Measurement
Control
Increased control flexibility due to FPGA interfacing capabilities
Increased versatility to be able to control different types of motors
Example reference designs showing how to use the control solution with Xilinx FPGAs
Where to Buy