This is an old revision of the document!
To get the system up and running follow the steps below:
The IIO Oscilloscope enables viewing the raw data acquired on all the ADC channels as well as controlling some hardware settings through the LiDAR plugin.
The main window of the IIO Osciloscope allows setting the length of the data captures and selecting the ADC channels that will be displayed on the plot. The length of the data capture must be always set to a multiple of 256 to match the internal data bus length, otherwise the plot will either hang or display incorrect data.
There are 5 channels under the axi-ad9094-hpc device, 4 of them (voltage0 to voltage3) corresponding to the physical data channels of the AD9094 and the 5th one (voltage4) showing the mux selections of the 4 TIAs on the AFE board. The mux selections channel is encoded on 8 bits with 2 bits for each TIA showing the actual bit values for the CHSEL0 and CHSEL1 TIA inputs. This channel is always selected. If it's interfering with the display of the other data channels it can always be multiplied with 0 using the Math function of the IIO oscilloscope.
A TIA channel sequencer implemented in the LiDAR HDL design that controls the mux selection independently for all the TIAs. The sequencer's operation can be controller from the LiDAR plugin using the options in the Sequencer Settings section. The sequencer can run in auto mode, meaning that it will change the mux selection at every data capture based on the sequence specified in the Auto Config section, which defines what the mux selection is for all the TIAs for 4 consecutive data captures. The length of the data capture is specified in the IIO Oscilloscope main window and a data capture is always triggered by the start of a laser pulse so that the start of the data is aligned with the transmitted laser pulse, which is time 0 for time of flight measurement.
In manual mode the 4 Manual Channel controls correspond to the 4 TIAs on the AFE board, starting with U2 on the left and continuing with U3, U4, U5 to the right. The values are in the range 0:3 and control the setting of the CHSEL0 and CHSEL1 pins of the TIAs.
The Pulse delay setting controls the delay between the time the TIA channel is changed a new laser pulse is generated. This delay is required to account for the time needed by the TIA to settle after the channel change.
The HDL design contains a pulse generator that precisely controls the timing of the laser pulses. The generator must be enabled before the data capture is started because the captures are triggered by the laser pulses. There are 2 parameters that can be controlled for the laser pulses - the frequency and the width, which actually define the total optical power of the system.
The system was certified for Eye Safety Class 1 with 20ns pulse width and 50KHz laser settings. When operating the system above these settings eye safety class 1 is not longer guaranteed and laser safety glasses (e.g LG2 laser safety glasses) must be worn all the time. It is recommended to wear laser safety glasses all the time irrespective of the laser setting to avoid any dangerous situations that might arise when modifying the software.
The APD on the AFE board needs a negative bias voltage in the range 120V to 200V to work. This determines the sensitivity of the APD and is set through the APD Bias control.
The TIA output signal has an offset that can be compensated via the Tilt control. This helps bring the signal close to 0 and maximize the ADC range.
See the AFE board wiki page for a complete description of the signal chain.
At system startup, besides the IIO Oscilloscope, the JESD 204B Eye Scan app starts to allow monitoring the status of the JESD204B link to the AD9094 on the DAQ board.