This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD-FMCDAQ3-EBZ on ZCU102
An Image file for ZynqMP (from zynqmp-common folder)
A BOOT.BIN specific to your AD-FMCDAQ3-EBZ + ZCU102
A system.dtb for ZynqMP specific to your AD-FMCDAQ3-EBZ + ZCU102
You will need to:
All the products described on this page include ESD (electrostatic discharge) sensitive devices. Electrostatic charges as high as 4000V readily accumulate on the human body or test equipment and can discharge without detection.
Although the boards feature ESD protection circuitry, permanent damage may occur on devices subjected to high-energy electrostatic discharges. Therefore, proper ESD precautions are recommended to avoid performance degradation or loss of functionality. This includes removing static charge on external equipment, cables, or antennas before connecting to the device.
Even thought this is Linux, this is a persistent file systems. Care should be taken not to corrupt the file system -- please shut down things, don't just turn off the power switch. Depending on your monitor, the standard power off could be hiding. You can do this from the terminal as well with sudo shutdown -h now
Analog Devices will provide limited online support for anyone using the reference design with Analog Devices components via the EngineerZone.