The EVAL-ADAQ23875 evaluation boards enable a simplified evaluation of the performance of the ADAQ23875 15MSPS, 16-bit, High Speed, Precision μModule Data Acquisition Solutions.
The ADAQ23875 μModule integrates crucial passive components with superior matching and drift characteristics to minimize temperature dependent error sources and to offer optimized performance. The fast settling of the ADC driver stage provides a unique solution for high channel count multiplexed signal chain architectures and control loop applications.
The following section contains the evaluation instructions for EVAL-ADAQ23875FMCZ evaluation board using IIO Oscilloscope.
The evaluation board consists of one μModule (U1, ADAQ23875, a choice of a 4.096V reference (U5, LTC6655) or 2.048V reference (U3, ADR4520), on-board power supplies to drive the necessary supply rails using the LTM8049 (U6), the ADP7118 (U4), the ADP7183 (U7), the LT3023 (U8), and an 800 MHz clock distribution IC (U13). The user also has an option to use the A2 and A3 amplifiers, such as the ADA4899-1, when evaluating the ADAQ23875.
The EVAL-ADAQ23875FMCZ can be powered from an external 3.3 V supply applied using the JP9 solder link if desired (see Table 2). The positive rails of the EVAL-ADAQ23875FMCZ, 7 V (+VS), 5 V (VDD), and 2.5 V (VIO), are generated from a combination of the power µModule, LTM8049 (U6), ADP7118 (U4), and a dual output low dropout (LDO) regulator, LT3023 (U8). The negative rail of the EVAL-ADAQ23875FMCZ, −2.0 V (−VS), is generated by a combination of the power µModule, LTM8049 (U6), and ADP7183 (U7). Each supply rail has necessary decoupling capacitors placed close to the device. A single ground plane is used on the board to minimize the effect of high frequency noise interference.
Table 1: On-Board Power Supplies
The Subminiature Version A (SMA) connectors (VIN+ and VIN−) on the EVAL-ADAQ23875FMCZ are used to provide analog inputs from a low noise, audio precision signal source (such as the SYS-2700 or the SYS-x555 series). There are three options available to feed analog inputs directly to the ADG774, ADA4899-1 and the ADAQ23875.
The optional amplifiers, ADA4899-1 (A2, A3), can be set up in a unity-gain configuration driving the ADAQ23875. In a default configuration of the EVAL-ADAQ23875FMCZ, an input signal via VIN+ and VIN- can be fed directly to the ADAQ23875 by bypassing U2, A2 and A3.
The EVAL-ADAQ23875FMCZ is factory configured to provide the appropriate input signal type, single-ended or fully differential, and different gain/attenuation or input range scaling. Table 2 lists the necessary jumper positions and link options for different configurations. The default board configuration presents a 4.096 V on the REFBUF pin and a buffered 2.048V (midscale) at the VCMO pin of the FDA on the ADAQ23875.
For low input frequency testing below 100 kHz, it is recommended to use a low noise, audio precision signal source (such as the SYS-2700 series) with the outputs set to balanced floating. A different precision signal source can be used alternatively with additional band-pass filtering. The filter bandwidth depends on input bandwidth of interest.
Multiple link options must be set correctly for the appropriate operating setup before applying the power and signal to the EVAL-ADAQ23875FMCZ. Refer to the link below for the link options for this evaluation boards.
Figure 2: Link Options for the EVAL-ADAQ23875FMCZ
The functional descriptions for all the connectors used on the EVAL-ADAQ23875FMCZ are listed in Table 3 and Table 4. There are several test points and single in line (SIL) headers on the EVAL-ADAQ23875FMCZ. These test points provide easy access to on-board signals for troubleshooting and evaluation purposes.
Table 3: On-Board Connectors
Table 4: 160-Pin FMC Connector (P5) Details
1 User defined signals with a P suffix can be used as the positive pin of the differential pair. User defined signals with an N suffix can be used as the negative pin of the differential pair. For further information, see the VITA 57 specification.
2 User defined signals with a CC suffix are the preferred signal lines on which to transmit clock signals from the controller board to the daughter board. These signal lines are connected to global clock lines on the FPGA, but they can also be used to carry any other user defined signal. For further information, see the VITA 57 specification.
To properly evaluate the EVAL-ADAQ23875, you need to ensure that the ADI Kuiper Linux is properly flashed on the SD card. Complete instructions on how to properly download, write and configure the image can be accessed at Kuiper Images. Make sure to comply with the directions for preparing the image for ADAQ23875.
Follow these steps to prepare the SD Card,
The Analog Devices Kuiper Linux image is an open-source, embedded Linux operating system based on Raspberry Pi OS. It incorporates Linux device drivers for ADI products as well as tools and other software products designed and created for ease of use.
Figure 2: Signal Chain Connection
Follow these steps to setup the complete system using Audio Precision Audio Analyzer as input source.
Once all steps are done, the IIO Oscilloscope software should run smoothly.
Each plugin (or tab) can be detached from the main window simply by clicking on the button placed on the right side of the name of the plugin. Close the detached window to attach the plugin back to the main window. The Main Window is designed to display a configuration panel (plugin) for each device recognized by the system. Additional plugins will be loaded for device debugging and monitoring purposes such as Debug Tab/Plugin and DMM Tab/Plugin.
Figure 3: Main Window
Debug Plugin is a tool for device debugging. Since “normal” users should not be doing this, features on this tab may not work unless you have started the osc application as root.
Figure 4: Debug Tab/Plugin
DMM Plugin: The Digital Multimeter continuously displays device specific data once the start button is activated.
Figure 5: DMM Tab/Plugin
The Capture Window is where device data is displayed.
Figure 6: Time Domain Plot
Figure 7: Frequency Domain Plot
Markers are used for plot data measurement when looking in the frequency domain or during cross correlation. To activate the markers, right click on the plot and select from the marker menu the type of marker you want to enable. Ensure that the capture process is running and the appropriate domain is selected in order to enable the markers properly. The following types of markers are available:
The enabling of a marker will display a set of 5 markers by default. You can add more markers by selecting Add Marker from the marker menu and remove some by selecting Remove Marker.
Once a data is captured, it can be saved using on of the following formats:
Figure 8: Save As Window
Make sure to download/update to the latest version of IIO-Oscilloscope.
https://github.com/analogdevicesinc/iio-oscilloscope/releases
To obtain the FFT plot, follow the ff steps:
The printed circuit board (PCB) layout is critical for preserving signal integrity and achieving the expected performance from the ADAQ23875. A multilayer board with an internal, clean ground plane in the first layer beneath the ADAQ23875 is recommended. Care must be taken with the placement of individual components and routing of various signals on the board. It is highly recommended to route input and output signals symmetrically. Solder the ground pins of the ADAQ23875 directly to the ground plane of the PCB using multiple vias. Remove the ground and power planes under the analog input/output and digital input/output (including F1 and F2) pins of the ADAQ23875 to avoid undesired parasitic capacitance. Any undesired parasitic capacitance can impact the distortion and linearity performance of the ADAQ23875.
The pinout of the ADAQ23875 eases the layout and allows its analog signals on the left side and its digital signals on the right side. The sensitive analog and digital sections must be separated on the PCB while keeping the power supply circuitry away from the analog signal path. Fast switching signals, such as CNV± or CLK±, and the DA± and DB± digital outputs must not run near or cross over analog signal paths to prevent noise coupling to the ADAQ23875.
Good quality ceramic bypass capacitors of at least 2.2 µF (0402,X5R) must be placed at the output of LDO regulators generating the µModule supply rails (VDD, VIO, VS+, and VS-) to GND to minimize electromagnetic interference (EMI) susceptibility and to reduce the effect of glitches on the power supply lines. All the other required bypass capacitors are laid out within the ADAQ23875, saving extra board space and cost. When the external decoupling capacitors on REFIN, VDD, and VIO pins near the µModule are removed, there is no significant performance impact.
The mechanical stress of mounting a device to a board can cause subtle changes to the SNR and internal voltage reference. The best soldering method is to use IR reflow or convection soldering with a controlled temperature profile. Hand soldering with a heat gun or a soldering iron is not recommended.
EVAL-ADAQ23875FMCZ Design and Integration Files
End of Document