EVALUATING THE AD9709/63/65/67 DIGITAL-TO-ANALOG CONVERTER
Preface
This user guide describes both the hardware and software setup needed to acquire data capture from AD9767-KIT-EBZ
to characterize AD9709/AD9763/AD9765/AD9767 dual-port, high speed, 2-channel, 8-/10-/12-/14-bit CMOS DACs.
This guide shows how the AD9767-KIT-EBZ works with SDP-H1 controller board developed by Analog Devices. Link to the previous user guide document is provided for customers who still have DPG2 and DPG3 controller boards.
Typical Setup
Figure 1. AD9767-KIT-EBZ Evaluation Setup
Tip: Click on any picture in this guide to open an enlarged version.
Helpful Files
Software Needed:
Hardware Needed:
-
-
12Vdc 1A Wall Adapter for SDP-H1
3Vdc power supply for the evaluation board.
PC with DPG Lite Software Application
High-Frequency Continuous Wave Generator (Clock Source)
Signal/Spectrum Analyzer
-
(3) SMA Cables
SMA T-connector
Quick Start Guide
-
-
Supply 3.3Vdc to the evaluation board and 12Vdc to the SDP-H1.
Using an SMA T-connector, split the output of a High-Frequency Clock Source (
e.g. SMA100A) to SMA J701 on SDP-H1 and to SMA S1 on the evaluation board. Set to 100MHz, 16dBm output.
Connect the spectrum analyzer to SMA S6 on the evaluation board.
Open DPG Downloader Lite. On the SDP-H1 Unit 1 Panel, select LVCMOS-3.3V on the Port Configuration. Double check if the DCO Frequency detected is 100MHz.
Click on the Add Generator Waveforms pulldown menu select Single Tone. Set the Data Rate to 100MHz and Desired Frequency to 5MHz. Check the Unsigned Data box and the Generate Complex Data (I & Q). Refer to Figure 2.
Select 16 bits
DAC Resolution for all generics (AD9767, AD9765, AD9763, and AD9709).
Figure 2. DPG Lite Session for AD9709/63/65/67 Evaluation Board]
Select the I/Q tone from the I/Q Data Vector pulldown menu.
Press the
Download arrow and then the
Play button. The spectrum similar to Figure 3 should appear in the signal/spectrum analyzer.
Figure 3. Spectrum Output for AD9767; Fdac = 100MSPS, Fout = 5MHz
Reconfiguring the Evaluation Board
This section details how to configure the AD9709/63/65/67 Evaluation Board and allow user to evaluate AD9709, AD9763 and AD9765. Set up the board as shown in figure 4.
To evaluate AD9709, Remove RP6 for DAC channel 1 and RP8 for DAC channel 2.
To evaluate AD9763, Remove RP6 for DAC channel 1 and RP8 for DAC channel 2 and add 2 22ohm resistors.
To evaluate AD9765, Remove RP6 for DAC channel 1 and RP8 for DAC channel 2 and add 4 22ohm resistors.
Figure 4. AD9709 | AD9763 | AD9765 LSB Configurations
Troubleshooting
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur:
Check the supply voltage of the evaluation board. Voltage rail should be 3.3V.
Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.
Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.
Power cycle both the SDP-H1 and the AD9709/6x evaluation board.
Check on the Spectrum Analyzer if the DAC clock inputs are properly driven. For 100MHz clock, the spectrum analyzer should detect a weak signal at 100MHz. If not detected, check properly the clock source and connections.
Disconnect and reconnect the SDP-H1 and AD9709/6x evaluation board. Reopen DPG Lite software.