No renderer 'pdf' found for mode 'pdf'
EVALUATING THE AD9146 DIGITAL-TO-ANALOG CONVERTER
Preface
This user guide describes both the hardware and software setup needed to acquire data capture from AD9146-M5375-EBZ evaluation board to characterize AD9146 dual 16-bit 1230 MSPS TxDAC+® digital-to-analog converter.
This guide shows how AD9146-M5375-EBZ works with SDP-H1 or ADS7-V2 controller board developed by Analog Devices. Link to the previous user guide document is provided for customers who still have the DPG3 controller board.
Typical Setup
Figure 1a. EVAL-AD9146 Setup with SDP-H1
Figure 1b. EVAL-AD9146 Setup with ADS7-V2
Tip: Click on any picture in this guide to open an enlarged version.
Helpful Files:
Software Needed:
Known Issue: ACE may fail to detect HS-DAC boards, details
here.
Hardware Needed:
-
-
AD-DAC-FMC-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
5Vdc 2A Power Supply
PC with ACE and DPG Lite Software Applications
High-Frequency Continuous Wave Generator
Signal/Spectrum Analyzer
-
(2) SMA Cables
The following are included in SDP-H1 Evaluation Kit:
The following are included in ADS7-V2 Evaluation Kit:
Quick Start Guide
Make sure that on the evaluation board, JP4, JP5, JP6, and JP7 are configured such that I and Q outputs are connected to the corresponding baluns (T7, T8). Refer to Figure 6. Configure JP10 and JP15 such that AD9146 clock input is connected to AD9516 clock divider/buffer. Refer to Figure 5.
Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J5 or J9 to a signal/spectrum analyzer. Connect the evaluation board to PC via
USB and to a 5Vdc 2A power supply via banana plug cables. Refer to Figures 1a and 1b.
If using
SDP-H1, set clock input to
100 MHz and 0 dBm. Connect SDP-H1 to PC via
USB and to a 12Vdc wall wart.
If using
ADS7-V2, set the clock input to
500 MHz and 0 dBm. Connect ADS7-V2 to PC via
USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.
Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9146 evaluation board. Apply the configuration wizard settings shown in Figure 2a for SDP-H1 and in Figure 2b for ADS7-V2.
Figure 2a. ACE Initial Configuration Wizard when using SDP-H1
Figure 2b. ACE Initial Configuration Wizard when using ADS7-V2
If using
SDP-H1, set
DAC frequency to 100
MHz,
Interpolation to 2x and
Data Format to binary format.
If using
ADS7-V2, set
DAC frequency to 500
MHz,
Interpolation to 2x and
Data Format to binary format.
In ACE, AD9146 on-chip
PLL can be enabled or not. To enable the on-chip
PLL check the
Enable PLL Clock in the wizard under
AD9146 PLL Setup. Select
Auto Mode for
PLL Mode option. The
PLL Locked LED on the ACE Board View should light up green. If the LED doesn't light up, try reapplying the wizard configuration and make sure that the VCO frequency is within the valid range of 1 - 2.1
GHz.
Start DPG Lite or DPG Downloader.
At the SDP-H1 part of the software, the device part number and
DCO frequency of around
100 MHz should be displayed.
At the ADS7-V2 part of the software, the device part number and
DCO frequency of around
500 MHz should be displayed.
In DPG Lite or DPG Downloader, from the Add Generator Waveforms pulldown menu, select Single Tone and apply the settings as shown in Figures 3a and 3b. The data rate in DPG software should be equal to the data rate in ACE.
When using SDP-H1, set
Data Rate to 50
MHz and
Desired Frequency to 10
MHz.
When using ADS7-V2, set
Data Rate to 250
MHz and
Desired Frequency to 21
MHz.
Continuing on setting up DPG Lite or DPG Downloader, set
DAC resolution to 16 bits. Check off the
Generate Complex Data (I & Q) box.
Figure 3a. DPG Lite session for SDP-H1
Figure 3b. DPG Lite session for ADS7-V2
Select the in-phase tone from the I Data Vector pulldown menu and the quadrature tone from the Q Data Vector pulldown menu.
Press the download arrow and then the play button. The FFT plots similar to Figures 4a and 4b should appear in the signal/spectrum analyzer.
Figure 4a. EVAL-AD9146 FFT for Data Rate = 50 MHz, Fout = 10 MHz
Figure 4b. EVAL-AD9146 FFT for Data Rate = 250 MHz, Fout = 21 MHz
Reconfiguring the Evaluation Board
Jumpers for Selecting the Clock Source
The AD9146 has an on-chip phase-locked loop (PLL) that uses the REFCLKP and REFCLKN pins to supply the reference clock. The AD9146-M5375-EBZ can supply the clock either from the AD9516-0 clock chip or from an additional external signal generator by connecting to J14. Connecting the inner pads to JP10 and JP15 selects the option to use the AD9146 by default, whereas soldering the outer pads chooses the external option to drive from a sine source.
Figure 5. DAC clock input is connected to AD9516 clock divider/buffer (default)
Jumpers for Selecting DAC Output Configuration
The AD9146-M5375-EBZ evaluates both the DAC I/Q outputs as well as the modulator RF outputs. Table 1 lists the jumper configurations and the SMA connections needed to view either the DAC IF outputs or the RF outputs on the spectrum analyzer.
The evaluation board has four three pad solder jumpers, two for each DAC (IOUT1N and IOUT1P, and IOUT2 N and IOUT2P). Use these solder jumpers, JP4 through JP7, to choose between viewing the DAC output or the modulator output. By default, the jumpers are configured to view the DAC output. For the modulator, solder the inner pads.
Figure 6. DAC I/Q Outputs to Baluns (default)
Hardware Provisions for Power Supplies
The AD9146-M5375-EBZ has five, two pin jumpers for each of the different power supplies on the board (see Table 2). By default, all of these jumpers must be populated.
Jumper for Transmit Enable pin
The AD9146 has a transmit enable feature (active low) that allows the user to control when the DACs transmit and when the outputs are clamped. This feature can be used by forcing a voltage on the TXENABLE pin via a test point. By default, the TXENABLE pin is set by the controller. Connect JP1 horizontally, as shown in Figure 7. To drive the TXENABLE pin manually, leave the jumper unsoldered.
Figure 7. TXENABLE Pin is connected to the controller (default)