This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ad9650-105ebz_ad9268-125ebz_ad9269-80ebz_ad9648-125ebz [22 Nov 2021 07:56] – [Design and Integration Files] Meriam Yuson-Aguila | resources:eval:ad9650-105ebz_ad9268-125ebz_ad9269-80ebz_ad9648-125ebz [03 Dec 2021 02:38] – [Troubleshooting Tips] Meriam Yuson-Aguila | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Typical Measurement Setup ===== | ===== Typical Measurement Setup ===== | ||
- | {{: | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
//Figure 1. Evaluation Board Connection—[[adi> | //Figure 1. Evaluation Board Connection—[[adi> | ||
Line 195: | Line 195: | ||
- Adjust the amplitude of the input signal so that the fundamental is at -1.0 dBFS. Examine the **Fund Power** reading in the left panel of the **VisualAnalog Graph - AD9268 Average FFT** window (see Figure 14) to verify this.{{ : | - Adjust the amplitude of the input signal so that the fundamental is at -1.0 dBFS. Examine the **Fund Power** reading in the left panel of the **VisualAnalog Graph - AD9268 Average FFT** window (see Figure 14) to verify this.{{ : | ||
- Repeat this procedure for Channel B. | - Repeat this procedure for Channel B. | ||
- | - Click the disk icon within the **Graph** window to save the performance plot data as .csv formatted file. See Figure 15 for an example.{{ : | + | - Click the disk icon within the **Graph** window to save the performance plot data as .csv formatted file. See Figure 15 for AD9268 |
- | | + | |
- | For Input Frequency fIN = 70 MHz, | + | |
- | SNRFS is equal to or greater than 77.2dBFS and typically equal to 78dBFS. | + | |
- | SFDR is equal to or greater than 85dBFS and typically equal to 88dBFS. | + | |
- | See Table 3 for desired results. | + | |
- | == Table 3. == | + | |
- | ^Family Name | + | |
- | |Fund Power* | + | |
- | |SNRFS | + | |
- | |SFDR |dBC |>83| | + | |
- | *Note: After adjusting Ain level on Signal Generator, on FFT Screen of Visual Analog | + | |
- | | + | |
===== Troubleshooting Tips ===== | ===== Troubleshooting Tips ===== | ||
If the FFT plot appears abnormal, do the following: | If the FFT plot appears abnormal, do the following: | ||
Line 227: | Line 216: | ||
- Make sure that all power and USB connections are secure. | - Make sure that all power and USB connections are secure. | ||
- Probe the DCOA signal at RN801 (Pin 2) on the evaluation board and confirm that a clock signal is present at the ADC sampling rate. | - Probe the DCOA signal at RN801 (Pin 2) on the evaluation board and confirm that a clock signal is present at the ADC sampling rate. | ||
+ | |||
+ | For AD9648 Family, it is worthwhile to perform Digital Reset if there is unexpected behavior to ensure that the ADC is initialized properly. | ||
+ | * SPI_Write (0x08, 0x03); #digital reset | ||
+ | * SPI_Write (0x08, 0x00); #normal operation | ||