This guide will walk you through the various features of the Analog Devices library for the ADIS16470 FRC IMU Board and how to use it in your robot code. If you're looking for a guide in another language, click here for LabVIEW or here for C++.
If you need help getting started with the basics of programming your robot in java, you may want to check out the WPI Screensteps documentation, which can be found here. Another useful resource can be found here.
In order to use the IMU, you will need to download and install the appropriate library. The instructions below assume you are using VS Code, the official supported development environment for FRC.
Before you can use the gyro in your code, you must first define an instance. Where exactly it needs to be defined will depend heavily on how your team organizes its robot code, but it needs to be accessible by the Robot class in order to work properly and give you no build errors. If your team is using an Iterative Robot with a RobotMap structure for example, you would put it inside of the RobotMap class. The ADIS16470 has its own dedicated class.
Because the IMU plugs directly into the SPI port, the library will pre-define your SPI port for you. IMU is a 3-axis sensor, so you will need to tell it which axis is the yaw axis. By default, this will be the Z axis if you don't define anything (this would be with the RoboRIO and the sensor sitting flat on or in the robot, facing up). Don't worry about defining an algorithm argument, the library will take care of this for you. A typical definition and instantiation will look like this:
public static final ADIS16470_IMU imu = new ADIS16470_IMU();
The IMU library will perform a calibration for you in its constructor, since this calibration MUST be performed in order for the IMU to function properly. The calibration inside of the constructor takes 4 seconds long by default, but you can change this by using the configCalTime() function. If you want to re-calibrate at some point in your code, you can call the calibrate() function. For more general information about offset calibration, please see the general ADIS16470 IMU page.
New for 2020, the calibrate() function now happens immediately when called. The ADIS16470 has an internal accumulation measurement which is applied as the new offset calibration value when calibrate() is called. Because of this, you should never run this command after the robot has started to move and should never be called after the robot start moving! This function is ideal for situations where the robot was powered on while moving during the initial calibration or if your robot has been sitting for a long time waiting for a match to start.
Now that your gyro is calibrated when the robot turns on, you can access data from the robot in your code. You can do this using the getAngle() method to obtain the robot's current yaw heading, or more rarely by using the getRate() method to obtain the current rotation rate being measured should you happen to need it. The most common places to use these functions are inside of the autonomousPeriodic() and teleopPeriodic() methods. By default, getAngle() returns the Y-axis angle, but you can change this by specifying a specific axis. If you know that your IMU will be mounted in such a way that the primary “yaw” axis is not the same as the IMU's Y axis, you can change the yaw axis by using setYawAxis().
Sometimes it may be necessary to reset the IMU gyro's “zero degrees” position. All gyros will have some amount of drift over time and it's physically impossible to calibrate out all sources of drift. In this case, you can use reset() to reset the current gyro heading to 0 degrees. When doing this, your robot should be facing the direction you want zero degrees to be, particularly if you are driving with field-oriented drive using an omnidirectional drive base. Otherwise, your robot may begin to behave incorrectly. For this reason, you should never automate this routine. Note that this does not recalibrate the gyro, so you don't have to be sitting still to perform this method properly.
The code block shown below is a modification of the WPI Library gyro drive straight example to use the ADIS16470 IMU instead.
/*----------------------------------------------------------------------------*/ /* Copyright (c) 2017-2018 FIRST. All Rights Reserved. */ /* Open Source Software - may be modified and shared by FRC teams. The code */ /* must be accompanied by the FIRST BSD license file in the root directory of */ /* the project. */ /*----------------------------------------------------------------------------*/ package org.usfirst.frc.team12333.robot; import com.analog.adis16470.frc.ADIS16470_IMU; import edu.wpi.first.wpilibj.IterativeRobot; import edu.wpi.first.wpilibj.Joystick; import edu.wpi.first.wpilibj.Spark; import edu.wpi.first.wpilibj.drive.DifferentialDrive; /** * This is a sample program to demonstrate how to use a gyro sensor to make a * robot drive straight. This program uses a joystick to drive forwards and * backwards while the gyro is used for direction keeping. */ public class Robot extends IterativeRobot { private static final double kAngleSetpoint = 0.0; private static final double kP = 0.005; // propotional turning constant // gyro calibration constant, may need to be adjusted; // gyro value of 360 is set to correspond to one full revolution private static final double kVoltsPerDegreePerSecond = 0.0128; private static final int kLeftMotorPort = 0; private static final int kRightMotorPort = 1; private static final int kJoystickPort = 0; private DifferentialDrive m_myRobot = new DifferentialDrive(new Spark(kLeftMotorPort), new Spark(kRightMotorPort)); private AnalogGyro m_gyro = new AnalogGyro(kGyroPort); private Joystick m_joystick = new Joystick(kJoystickPort); public static final ADIS16470_IMU imu = new ADIS16470_IMU(); @Override public void robotInit() { // You can put a calibrate() method call here, but it's not necessary since the library does it for you } /** * The motor speed is set from the joystick while the RobotDrive turning * value is assigned from the error between the setpoint and the gyro angle. */ @Override public void teleopPeriodic() { double turningValue = (kAngleSetpoint - imu.getAngle()) * kP; // Invert the direction of the turn if we are going backwards turningValue = Math.copySign(turningValue, m_joystick.getY()); m_myRobot.arcadeDrive(m_joystick.getY(), turningValue); } }