Wiki

This version (31 Jan 2020 01:55) was approved by Kristen Chong.The Previously approved version (10 Jan 2020 04:54) is available.Diff

Using the ADIS16470 IMU Board for FRC in C++

This guide will walk you through the various features of the Analog Devices library for the ADIS16470 FRC IMU Board and how to use it in your robot code. If you're looking for a guide in another language, click here for Java or here for LabVIEW.

If you need help getting started with the basics of programming your robot in C++, you may want to check out the WPI Screensteps documentation, which can be found here. Another useful resource can be found here.

Installing the Library

In order to use the IMU, you will need to download and install the appropriate library from GitHub. The instructions below assume you are using VS Code, the official supported development environment for FRC.

Offline Install

  1. Download the latest release zip from this page. The zip will be named adis16448_roborio-[releaseversion].zip.
  2. Close all instances of FRC Visual Studio Code
  3. If using Windows, extract the zip you downloaded to C:\Users\Public\frc2019. If using Linux or Mac, extract the zip to ~/home/frc2019/.
  4. Open FRC Visual Studio Code
  5. Click the WPILib command pallete icon
  6. Select “Manage Vendor Libraries” in the menu
  7. Choose “Install New Libraries (Offline)”
  8. Check ADIS16470, then click “OK”.



Instance Definition and Instantiation

Before you can use the gyro in your code, you must first define an instance. Where exactly it needs to be defined will depend heavily on how your team organizes its robot code, but it needs to be accessible by the Robot class in order to work properly and give you no build errors. If your team is using an Iterative Robot with a RobotMap structure for example, you would put it inside of the RobotMap class. The ADIS16470 has its own dedicated class in its own namespace.

Because the IMU plugs directly into the SPI port, the library will pre-define your SPI port for you. A typical definition and instantiation will look like this:

frc::ADIS16470_IMU imu{};



Sensor Initialization/Calibration with Calibrate()

The IMU library will perform a calibration for you in its constructor, since this calibration MUST be performed in order for the IMU to function properly. The calibration inside of the constructor takes 4 seconds long by default, but you can change this by using the ConfigCalTime() function. If you want to re-calibrate at some point in your code, you can call the Calibrate() function. For more general information about offset calibration, please see the general ADIS16470 IMU page.

New for 2020, the Calibrate() function now happens immediately when called. The ADIS16470 has an internal accumulation measurement which is applied as the new offset calibration value when Calibrate() is called. Because of this, you should never run this command after the robot has started to move! This function is ideal for situations where the robot was powered on while moving during the initial calibration or if your robot has been sitting for a long time waiting for a match to start.

Using GetAngle() and GetRate()

Now that your gyro is calibrated when the robot turns on, you can access data from the robot in your code. You can do this using the GetAngle() method to obtain the robot's current yaw heading, or more rarely by using the GetRate() method to obtain the current rotation rate being measured should you happen to need it. The most common places to use these functions are inside of the AutonomousPeriodic() and TeleopPeriodic() methods. By default, GetAngle() returns the Y-axis angle, but you can change this by specifying a specific axis. If you know that your IMU will be mounted in such a way that the primary “yaw” axis is not the same as the IMU's Y axis, you can change the yaw axis by using SetYawAxis().

As a general note, the GetAngle() functions will count continuously, meaning when they reach 360 degrees, they will continue to 361, not zero. This is to make any functionality in your code using the IMU angle easier to implement without having to keep track of where in the 0-360 range your robot is or how many rotations have happened.



Re-Zeroing the Sensor with Reset()

Sometimes it may be necessary to reset the IMU gyro's “zero degrees” position. All gyros will have some amount of drift over time and it's physically impossible to calibrate out all sources of drift. In this case, you can use Reset() to reset the current gyro heading to 0 degrees. When doing this, your robot should be facing the direction you want zero degrees to be, particularly if you are driving with field-oriented drive using an omnidirectional drive base. Otherwise, your robot may begin to behave incorrectly. For this reason, you should never automate this routine. Note that this does not recalibrate the gyro, so you don't have to be sitting still to perform this method properly.

Drive Straight Example

The code block shown below is a modification of the WPI Library gyro drive straight example to use the ADIS16470 IMU instead.

/*----------------------------------------------------------------------------*/
/* Copyright (c) 2017-2018 FIRST. All Rights Reserved.                        */
/* Open Source Software - may be modified and shared by FRC teams. The code   */
/* must be accompanied by the FIRST BSD license file in the root directory of */
/* the project.                                                               */
/*----------------------------------------------------------------------------*/

#include <cmath>

#include <Drive/DifferentialDrive.h>
#include <IterativeRobot.h>
#include <Joystick.h>
#include <Spark.h>
#include <ADIS16470_IMU.h>

/**
 * This is a sample program to demonstrate how to use a gyro sensor to make a
 * robot drive straight. This program uses a joystick to drive forwards and
 * backwards while the gyro is used for direction keeping. This code assumes
 * that your yaw axis is the X axis.
 */
class Robot : public frc::IterativeRobot {
public:
	
	ADIS16470_IMU imu*;
	
	void RobotInit() override {
		imu.Calibrate();
                imu.SetYawAxis(kX);
	}

	/**
	 * The motor speed is set from the joystick while the DifferentialDrive
	 * turning value is assigned from the error between the setpoint and the
	 * gyro angle.
	 */
	void TeleopPeriodic() override {
		double turningValue = (kAngleSetpoint - imu.GetAngle()) * kP;
		// Invert the direction of the turn if we are going backwards
		turningValue = std::copysign(turningValue, m_joystick.GetY());
		m_robotDrive.ArcadeDrive(m_joystick.GetY(), turningValue);
	}

private:
	static constexpr double kAngleSetpoint = 0.0;
        static constexpr double kP = 0.005;

	static constexpr int kLeftMotorPort = 0;
	static constexpr int kRightMotorPort = 1;
	static constexpr int kJoystickPort = 0;

	frc::Spark m_left{kLeftMotorPort};
	frc::Spark m_right{kRightMotorPort};
	frc::DifferentialDrive m_robotDrive{m_left, m_right};
        frc::ADIS16470_IMU imu{};

	frc::Joystick m_joystick{kJoystickPort};
};

START_ROBOT_CLASS(Robot)
first/adis16470_imu_frc/cpp.txt · Last modified: 31 Jan 2020 01:55 by Kristen Chong