Both sides previous revisionPrevious revisionNext revision | Previous revision |
university:tools:uartjtag:hardware [01 Feb 2019 21:24] – fixed broken link Brandon Bushey | university:tools:uartjtag:hardware [29 Jan 2021 09:36] (current) – Fixed bad link for digikey Ioana Chelaru |
---|
====== ADALM-UARTJTAG hardware ====== | ====== ADALM-UARTJTAG hardware ====== |
| |
In many different boards, we include this: | Analog Devices provides a small adapter board [[../uartjtag|(ADALM-UARTJTAG)]] to be used for JTAG and UART, in order to make that easier for programming and debugging. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V. |
| |
{{:university:tools:jtaguart:schematic.png?direct&300|}} | In the box, you should have received the UARTJTAG board, ribbon cable, jumper, and [[https://www.samtec.com/products/ftsh|Samtec FTSH-105-01-L-D 10]] position dual row 0.05" through hole pin connector. |
| |
which allows a small adapter to be used for JTAG and UART, in order to make that easier for people, we optionally allow people to purchase the [[../uartjtag|ADALM-UARTJTAG]] adapter. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V. | {{ :university:tools:jtaguart:adalm-uartjtag.png?400 |}} |
| |
In the box, you should have received the UARTJTAG board, ribbon cable, USB cable, and [[https://www.samtec.com/products/ftsh|Samtec FTSH-105-01-L-D 10]] position dual row 0.05" through hole pin connector. | |
| |
{{:university:tools:jtaguart:uartjtag.png?direct&550|1 }} | |
{{ :university:tools:jtaguart:uartjtag.boardpng.png?direct&200|5}} | |
| |
The PCB includes a jumper, which forces the Zynq to HALT on JTAG. This is great for halting, and not allowing anything to run, but does does pull down a chip select for SPI flash, and will not allow the SPI flash to be found by the on chip bootloader, or by U-Boot. (If you are loading a U-Boot over JTAG). | The PCB includes a jumper, which forces the Zynq to HALT on JTAG. This is great for halting, and not allowing anything to run, but does does pull down a chip select for SPI flash, and will not allow the SPI flash to be found by the on chip bootloader, or by U-Boot. (If you are loading a U-Boot over JTAG). |
| |
If you do want more, they can be obtained from [[https://www.samtec.com/products/ftsh-105-01-l-d|Samtec]], | If you do want more, they can be obtained from [[https://www.samtec.com/products/ftsh-105-01-l-d|Samtec]], |
[[https://www.digikey.com/product-detail/en/samtec-inc/FTSH-105-01-L-D/SAM10499-ND/2649978|Digikey]] or [[https://www.arrow.com/en/products/ftsh-105-01-l-d/samtec|Arrow]]. | [[digikey>SAM10499-ND|Digikey]] or [[https://www.arrow.com/en/products/ftsh-105-01-l-d/samtec|Arrow]]. |
| |
====== Downloads ====== | ====== Downloads ====== |
* {{:university:tools:jtaguart:adalm-jtaguart_fab.zip|Rev A Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) | * {{:university:tools:jtaguart:adalm-jtaguart_fab.zip|Rev A Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) |
* {{:university:tools:jtaguart:adalm-jtaguart.xlsx|Rev A Bill of materials}} | * {{:university:tools:jtaguart:adalm-jtaguart.xlsx|Rev A Bill of materials}} |
* {{:university:tools:jtaguart:adalm-jtaguart_brd.zip|Rev A Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[http://www.cadence.com/products/pcb/Pages/downloads.aspx|Allegro FREE Physical Viewer]] to view. | * {{:university:tools:jtaguart:adalm-jtaguart_brd.zip|Rev A Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]] to view. |
| </WRAP> |
| |
| <WRAP round download 65%> |
| * {{|Rev B Schematics}} |
| * {{|Rev B Gerbers}} (This file is [[http://www.7-zip.org/7z.html|compressed]]) |
| * {{|Rev B Bill of materials}} |
| * {{|Rev B Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]] to view. |
</WRAP> | </WRAP> |
| |