Analog Devices provides a small adapter board (ADALM-UARTJTAG) to be used for JTAG and UART, in order to make that easier for programming and debugging. You are encouraged to use this on your designs for the same reason we do - the standard JTAG connector is huge, and there are times where good old fashion console UART is valuable for doing debug. The 1.8V supply on the connector above is the I/O voltage, and can be used anywhere between 1.8V and 3.3V.
In the box, you should have received the UARTJTAG board, ribbon cable, jumper, and Samtec FTSH-105-01-L-D 10 position dual row 0.05“ through hole pin connector.
The PCB includes a jumper, which forces the Zynq to HALT on JTAG. This is great for halting, and not allowing anything to run, but does does pull down a chip select for SPI flash, and will not allow the SPI flash to be found by the on chip bootloader, or by U-Boot. (If you are loading a U-Boot over JTAG).
The pin connector is likely inserted into the ribbon cable:
but can be removed, and either soldered to the PCB, or left in the ribbon cable, so you don't loose it.
If you do want more, they can be obtained from Samtec, Digikey or Arrow.