Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:tools:pluto:users [10 Mar 2017 22:00] – add receiver sensitivity Robin Getzuniversity:tools:pluto:users [20 Feb 2023 17:37] (current) – Added letter of volatility Brian OLoughlin
Line 3: Line 3:
 {{  :university:tools:pluto:pluto_in_hand.png?200|}} {{  :university:tools:pluto:pluto_in_hand.png?200|}}
  
-Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).+Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc.) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product).
  
 ===== Contents ===== ===== Contents =====
Line 10: Line 10:
     - [[./users/name|What's with the name?]] //PlutoSDR?//     - [[./users/name|What's with the name?]] //PlutoSDR?//
     - [[./users/understanding|Understanding the Internals]]     - [[./users/understanding|Understanding the Internals]]
-    - [[./users/transmit|RF Output]] +    - [[./users/temp|How hot?]] 
-    - [[./users/receive|RF Input]] +    - [[./users/far_fast|How Far, How fast?]] 
-      - [[./users/receiver_sensitivity|Receiver Sensitivity]]+      - [[./users/transmit|RF Output]] 
 +        - [[./users/phase_noise|Phase Noise & Accuracy]] 
 +      - [[./users/receive|RF Input]] 
 +        - [[./users/receiver_sensitivity|Receiver Sensitivity]] 
 +        - [[./users/non_quad|Dealing with Non-Quadrature signals]]
     - [[./users/antennas|Antennas]]     - [[./users/antennas|Antennas]]
 +    - {{./users/letter_of_volatility_pluto.pdf|Letter of Volatility}}
   - [[./users/quick_start|Quick Start]]   - [[./users/quick_start|Quick Start]]
   - Intro to the Software. Installing Device Drivers on:   - Intro to the Software. Installing Device Drivers on:
Line 22: Line 27:
   - [[./users/calibration|Calibrating]] the ADALM-PLUTO.   - [[./users/calibration|Calibrating]] the ADALM-PLUTO.
   - [[./users/customizing|Customizing]] the ADALM-PLUTO.   - [[./users/customizing|Customizing]] the ADALM-PLUTO.
-    - using more than one the ADALM-PLUTO on the same PC. 
   - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from:   - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from:
-    - Using Pluto with the [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] +    - [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] 
-      - example 1 +    - [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio 
-    - Using Pluto with the [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio and the Qt graphical toolkit+    - [[mw>hardware-support/adalm-pluto-radio.html|Official support for MATLAB and Simulink]]  
-    - Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB]]  +    - [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB IIO Bindings]] 
-      - example 1 +    - [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] 
-    - Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|Simulink]] +    - [[https://github.com/f4exb/sdrangel|SDRangel]], an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. 
-      example 2 +    [[https://airspy.com/download/|SDR#]]. The PlutoSDR frontend for SDRsharp can be found here: [[https://github.com/Manawyrm/sdrsharp-plutosdr|sdrsharp-plutosdr]] 
-    - Using Pluto with [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] +    - [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://github.com/jocover/SoapyPlutoSDR|SoapyPlutoSDR]] 
-      example 1+    - [[https://github.com/radiosd/PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]]    
 +    - [[:resources/tools-software/linux-software/pyadi-iio|Python Interfaces]] 
 +    [[:university/tools/pluto/controlling_the_transceiver_and_transferring_data|C Examples]] 
 +  - [[Accessories]] 
 +  - [[ASEE Papers]]
  
  
  
university/tools/pluto/users.txt · Last modified: 20 Feb 2023 17:37 by Brian OLoughlin