This is an old revision of the document!
This may seem to be a puzzling topic to some — the radio is quadrature — how can a signal be non-quadrature?
The answer involves a little math, so the reader is expected to understand fundamental of quadrature signals. In the basic sense, quadrature signals can be broken down into two orthogonal components or source (modulated) sinusoids. Real or non-quadrature signals are technically a subset of quadrature when the components are in-phase or one of the components is zero. This is easy to observe spectrally since real-valued signals are conjugate symmetric in frequency. By only using quadrature, sometimes referred to as complex, a signal can we place information uniquely on a single sideband.
Transmitting a “real” signal isn't a problem. It's either:
In IIO-Scope, we can create a real signal by playing the same tone, at the same frequency, same magnitude out the DDSes all the same time.
Euler says that this should generate an equal-sized tone on each side of the LO, and we can check this by putting the part into digital loopback mode (anything that we send out the Tx, is sent to the Rx) by going to the advanced tab, under the Built-in Self Test (BIST) tab:
By looking at the time and frequency domain of the signal we are sending, we can see even after 300 years, the math holds up. (The time domain signal looks like only one (green = I
), since the other channel (red = Q
) is exactly the same and behind it.
You can achieve the same result mathematically by only sending I or Q (and sending zeros on the other channel). Here we set the magnitude on Q to -99 (or -Infinity).
The rest of the tests are the same as the above. Take note that even though we are sending the same magnitude of I as before, the power in the signal is less (the peaks in the FFT drop), since we are sending half the power, (only I, no Q).
We can send that out the RF, by disabling loopback and setting the Rx and Tx LO to the same value.
Receiving is where things can be more complicated. Most (all) integrated transceivers include some sort of Quadrature tracking corrections which try to ensure the signals are correct, and any imperfections in the chip or external circuitry (balun, non-differential traces, etc) are removed.
While the frequency domain plot does look close to the same, but we can see that the amplitude is jumping up and down by a few dB. (which is impossible to show in a static picture like this).
Its easier to look at this in the time domain. Here the amplitude difference between I & Q is random based on the random difference between the phase of the Rx and Tx PLL. This is indeed completely random, and will change any time either PLL settings are touched. Moving one LO to a different settings, and back again, will change this phase offset (which manifest itself as a magnitude difference between I and Q).
You can change this magnitude difference digitally by post processing the sampled data, by using the Phase Rotation control in IIO oscilloscope. It doesn't change the phase relationship between I and Q, but does change the effective sample time relative to the PLL, and therefore changes their relative magnitude. By changing this, you can effectively make either of the I or Q zero, and only receive the signal the other (Q or I), indicating that the received signal is “real” (all information can be received just on one signal channel, and it has no phase or quadrature information.
The easiest way to ignore these things is to look at the overall magnitude of the signal ie - set up a math equation in IIO-Scope with ssqrtf((voltage0*voltage0)+(voltage1*voltage1))*((voltage0 > 0)-(voltage0 < 0))
. This is the equivalent the . This will ensure that any I/Q magnitude difference doesn't affect the investigation.
You can see from the data (and the math) that we can rotate I/Q and it doesn't change the overall attitude of the signal.
By capturing 1048576 samples (or at 3MSPS, 349525.333 us) you can see what looks like some weird sort of steps. These perturbations are caused by two state machines inside the AD9363 fighting against each other. (1) Automatic Gain Control (ACG) and (2) Quadrature tracking corrections.
Here the green signal is the I, and the blue is the overall magnitude. Since, during this run, the I was showing most the the perturbations, and it is small compared to Q, the overall magnitude does not change that much, but it does have undesired step changes, that can be easily fixed when we understand what is happening.
The first step is to understand that the ACG is reacting to magnitude changes caused by the Quadrature tracking corrections. Turning the ACG to manual mode can help isolate the effects of the IQ Correction. Here is a picture of the same setup with the ACG set to manual mode.
Here we can see multiple times where the Quadrature tracking corrections are trying to suppress what it believes is an image until it gives up, resets, and starts over. This results in what appears to be amplitude errors in the signal.
The problem statement is simple - there is no way for a Quadrature tracking correction algorithm to understand if a “real” signal is being sent, or if in fact something is quadrature, is an image, and needs to be suppressed. The only thing that understands that is the sentient being between the chair and the keyboard.
The easiest way to remove this error is to simply turn off Quadrature tracking corrections.
This will resolve the set changes in magnitude in either I or Q
The easiest way to look at things is via the magnitude of the signal ie - set up a math equation in IIO-Scope with sqrtf((voltage0*voltage0)+(voltage1*voltage1))
. This will ensure that any I/Q phase difference doesn't affect the results. Here when Rx and Tx PLL are the same, we can see the same issue.
Moving 1 kHz off (with Quadrature tracking On), makes the magnitude look like (which is the correct, expected result - constant magnitude over time):
It's expected there may be “waves” in the magnitude, as we are sending sinusoidal signals, and sampling at an offset will cause low-frequency aliasing. The best thing to do is to look at the signal with Quadrature tracking On and Off to see if it makes a difference. (all tests were taken with ACG turned off, so we are isolating one (Quadrature tracking) issue).
You can see from this that as long as you are off by 10 Hz or more, the Quadrature tracking feature works properly. In most systems, it's pretty rare to see this in the wild - as, at 2.4 GHz, a sub 10 Hz offset would be better than 4 parts per billion (or 0.004 ppm) offset. Unless you have a great reference clock, and spend some time tuning the system, and are lucky - you should never run into this.
It is quite easy to connect Rx to Tx and see this on the same unit - since the reference offset is 0 between Tx and Rx.
The IIO attributes that were used above are:
# iio_attr -a -c ad9361-phy RX_LO frequency dev 'ad9361-phy', channel 'altvoltage0' (output), id 'RX_LO', attr 'frequency', value '435000000' # iio_attr -a -c ad9361-phy TX_LO frequency dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'frequency', value '435000000' # iio_attr -D ad9361-phy loopback dev 'ad9361-phy', debug attr 'loopback', value :'0' # iio_attr -c ad9361-phy voltage0 gain_control_mode dev 'ad9361-phy', channel 'voltage0' (input), attr 'gain_control_mode', value 'manual' # iio_attr -c ad9361-phy voltage0 quadrature_tracking_en dev 'ad9361-phy', channel 'voltage0' (input), attr 'quadrature_tracking_en', value '1'
For those using a National Instruments USRP Radio, this can be controlled via set_rx_iq_balance()
method.
This issue will exist on all integrated devices which have some sort of Quadrature tracking feature, including all hardware based on ADI and other manufactures. It's not something specific to the ADALM-PLUTO, or the AD9363.