This is an old revision of the document!
Make sure the following drivers are installed:
The drivers and files should be compatible with:
A reboot is required after installing the HoRNDIS.
adi-mm:tests analogdevices$ ls -l /dev/tty.* crw-rw-rw- 1 root wheel 17, 0 Nov 7 15:13 /dev/tty.Bluetooth-Incoming-Port crw-rw-rw- 1 root wheel 17, 2 Nov 7 15:28 /dev/tty.usbmodem1414 adi-mm:tests analogdevices$ screen /dev/tty.usbmodem1414 115200 Welcome to Pluto pluto login: root Password: analog # uname -a Linux pluto 4.6.0-08511-gc1315e6-dirty #247 SMP PREEMPT Mon Oct 24 16:46:25 CEST 2016 armv7l GNU/Linux # CNTRL-A CNTRL-\ Really quit and kill all your windows [y/n] y [screen is terminating] adi-mm:tests analogdevices$
adi-mm:tests analogdevices$ mount | grep Pluto /dev/disk1s1 on /Volumes/PlutoSDR (msdos, local, nodev, nosuid, noowners)
Like most of the network settings on Pluto or the M2k - things are meant to be easy to use. This also means things are inherently insecure.
For example - the root password of Pluto is analog
. We post it on the Internet. Think about that for a moment. This could allow anyone with an IP connection to take over the device and use it for malicious purposes.
Never set up a bridge between the Internet and a network connected Pluto with the default images.
Unfortunately - nothing on your host understands the what the IP address of the usb device is. You, the human behind the keyboard need to understand this before any sort of networking will work. There are two main ways to do this:
Once the HoRNDIS driver is installed, you should see something like this when you goto → System Preferences → Network.
You may need to reboot without the PlutoSDR plugged in, and then attach the PlutoSDR to get HoRNDIS to load properly
To check things out, it should look something like this in dmesg
:
adi-mm:build analogdevices$ sudo dmesg HoRNDIS: init: HoRNDIS tethering driver for Mac OS X, by Joshua Wise (rel8 final) HoRNDIS: probe: probe: came in with a score of 60000 HoRNDIS: message: unknown message type e000401f HoRNDIS: message: unknown message type e0000230 HoRNDIS: probe: probe: looks like we're good (2/2/255) USBMSC Identifier (non-unique): 100000235523730700230012090216da47 0x456 0xb673 0x406, 2 HoRNDIS: message: kIOMessageServiceIsAttemptingOpen HoRNDIS: openInterfaces: data interface: okay, I got one, and it was a 0x0a/0x00/0x00 HoRNDIS: message: kIOMessageServiceIsAttemptingOpen HoRNDIS: rndisInit: their MTU 1486 HoRNDIS: setMaxTransferUnit: Excuse me, but I said you could have an MTU of 1486, and you just tried to set an MTU of 1500. Good try, buddy. HoRNDIS: init: starting up with MTU 1486 en4: attached with 4 suspended link-layer multicast membership(s) HoRNDIS: message: kIOMessageServiceIsAttemptingOpen HoRNDIS: message: kIOMessageServiceIsRequestingClose HoRNDIS: message: kIOMessageServiceIsAttemptingOpen HoRNDIS: message: kIOMessageServiceIsRequestingClose en4: failed to restore 4 suspended link-layer multicast membership(s) (err=102)
adi-mm:tests analogdevices$ ifconfig | grep -B 3 -A 3 192 en4: flags=8863<UP,BROADCAST,SMART,RUNNING,SIMPLEX,MULTICAST> mtu 1486 ether 00:e0:22:6d:b2:d8 inet6 fe80::2e0:22ff:fe6d:b2d8%en4 prefixlen 64 scopeid 0xa inet 192.168.2.10 netmask 0xffffff00 broadcast 192.168.2.255 nd6 options=1<PERFORMNUD> media: autoselect status: active
Adding a quick/short ssh config file, which describes the USB device can be helpful. It's maintained in github, and it's a simple matter of grabbing the raw text file. You shouldn't do the exact below unless you have no ~/.ssh/config
file. Otherwise, click on this link and copy/paste it into the system wide /etc/ssh/ssh_config
file, or the user specific ~/.ssh/config
file.
analog@imhotep:~$ wget https://raw.githubusercontent.com/analogdevicesinc/plutosdr_scripts/master/ssh_config -O ~/.ssh/config --2017-01-26 19:47:51-- https://raw.githubusercontent.com/analogdevicesinc/plutosdr_scripts/master/ssh_config Resolving raw.githubusercontent.com (raw.githubusercontent.com)... 151.101.116.133 Connecting to raw.githubusercontent.com (raw.githubusercontent.com)|151.101.116.133|:443... connected. HTTP request sent, awaiting response... 200 OK Length: 366 [text/plain] Saving to: ‘~/.ssh/config’ ~/.ssh/config 100%[===============>] 366 --.-KB/s in 0s 2017-01-26 19:47:51 (6.49 MB/s) - ‘~/.ssh/config’ saved [366/366]
Since the ssh key on the pluto changes every boot, we want to be able to never store the key (so we store it to /dev/null
. This does make it easier to use (don't need to continually edit the known_hosts
file), but does make things susceptible to man in the middle attacks.
adi-mm:tests analogdevices$ ssh plutosdr Warning: Permanently added 'pluto' (ECDSA) to the list of known hosts. root@pluto's password: analog # uname -a Linux pluto 4.6.0-08511-gc1315e6-dirty #247 SMP PREEMPT Mon Oct 24 16:46:25 CEST 2016 armv7l GNU/Linux # exit Connection to 192.168.2.1 closed. adi-mm:tests analogdevices$
if you have sshpass
installed, you can use that so you dont need to type in a password:
analog@imhotep:~/pluto$ sshpass -panalog ssh plutosdr Warning: Permanently added 'pluto' (ECDSA) to the list of known hosts. Welcome to: ______ _ _ _________________ | ___ \ | | | / ___| _ \ ___ \ | |_/ / |_ _| |_ ___ \ `--.| | | | |_/ / | __/| | | | | __/ _ \ `--. \ | | | / | | | | |_| | || (_) /\__/ / |/ /| |\ \ \_| |_|\__,_|\__\___/\____/|___/ \_| \_| http://wiki.analog.com/university/tools/pluto #