This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:pluto:drivers:osx [11 Apr 2017 22:05] – add m2k Robin Getz | university:tools:pluto:drivers:osx [07 Sep 2023 16:17] (current) – [Ethernet] Remove HoRNDIS Michael Hennerich | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Mac OS X Drivers ====== | ====== Mac OS X Drivers ====== | ||
- | Make sure the following drivers are installed: | ||
- | * [[http:// | ||
- | The drivers and files should be compatible with: | ||
- | * macOS El Capitan 10.11 | ||
- | * macOS Yosemite 10.10 | ||
- | A reboot is required after installing the HoRNDIS. | ||
===== Serial ===== | ===== Serial ===== | ||
Line 42: | Line 36: | ||
===== Ethernet ===== | ===== Ethernet ===== | ||
+ | |||
+ | <WRAP tip> | ||
+ | In order to use the ADALM-PLUTO (aka. PlutoSDR) or ADALM2000 (aka. M2k) with Mac OSX the ethernet compatibility mode must be set to **USB CDC-NCM**. | ||
+ | |||
+ | Please see instructions for [[: | ||
+ | </ | ||
{{page> | {{page> | ||
- | Once the [[http:// | + | You should see something like this when you goto -> System Preferences -> Network. |
- | + | ||
- | <WRAP tip>You may need to reboot without the PlutoSDR plugged in, and then attach the PlutoSDR to get HoRNDIS to load properly</ | + | |
{{: | {{: | ||
- | To check things out, it should look something like this in '' | ||
- | |||
- | <WRAP box> | ||
- | < | ||
- | adi-mm: | ||
- | HoRNDIS: init: HoRNDIS tethering driver for Mac OS X, by Joshua Wise (rel8 final) | ||
- | HoRNDIS: probe: probe: came in with a score of 60000 | ||
- | HoRNDIS: message: unknown message type e000401f | ||
- | HoRNDIS: message: unknown message type e0000230 | ||
- | HoRNDIS: probe: probe: looks like we're good (2/2/255) | ||
- | USBMSC Identifier (non-unique): | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: openInterfaces: | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: rndisInit: their MTU 1486 | ||
- | HoRNDIS: setMaxTransferUnit: | ||
- | HoRNDIS: init: starting up with MTU 1486 | ||
- | en4: attached with 4 suspended link-layer multicast membership(s) | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: message: kIOMessageServiceIsRequestingClose | ||
- | HoRNDIS: message: kIOMessageServiceIsAttemptingOpen | ||
- | HoRNDIS: message: kIOMessageServiceIsRequestingClose | ||
- | en4: failed to restore 4 suspended link-layer multicast membership(s) (err=102) | ||
- | </ | ||
- | </ | ||
<WRAP box> | <WRAP box> |