This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:pluto:drivers:osx [11 Apr 2017 22:05] – add m2k Robin Getz | university:tools:pluto:drivers:osx [23 Feb 2021 16:49] – Cristina Suteu | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Mac OS X Drivers ====== | ====== Mac OS X Drivers ====== | ||
+ | <WRAP info> | ||
+ | HoRNDIS is required for Remote Network Driver Interface Specification (RNDIS) which is a USB protocol to provides a virtual Ethernet link. If you don't want to access your device over network - don't install HoRNDIS. It is optional. | ||
+ | </ | ||
Make sure the following drivers are installed: | Make sure the following drivers are installed: | ||
- | * [[http:// | + | * [[http:// |
The drivers and files should be compatible with: | The drivers and files should be compatible with: | ||
+ | * macOS Mojave 10.14 | ||
+ | * macOS High Sierra 10.13 | ||
+ | * macOS Sierra 10.12 | ||
* macOS El Capitan 10.11 | * macOS El Capitan 10.11 | ||
* macOS Yosemite 10.10 | * macOS Yosemite 10.10 | ||
A reboot is required after installing the HoRNDIS. | A reboot is required after installing the HoRNDIS. | ||
+ | |||
+ | For newer macOS versions(from macOS Catalina 10.15 and up), HoRNDIS no longer provides official support. | ||
+ | |||
===== Serial ===== | ===== Serial ===== |