Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
university:tools:pluto:drivers:osx [11 Apr 2017 22:05] – add m2k Robin Getz | university:tools:pluto:drivers:osx [29 Jul 2020 01:47] – add note about HoRNDIS Robin Getz |
---|
====== Mac OS X Drivers ====== | ====== Mac OS X Drivers ====== |
| |
| <WRAP info> |
| HoRNDIS is required for Remote Network Driver Interface Specification (RNDIS) which is a USB protocol to provides a virtual Ethernet link. If you don't want to access your device over network - don't install HoRNDIS. It is optional. |
| </WRAP> |
Make sure the following drivers are installed: | Make sure the following drivers are installed: |
* [[http://joshuawise.com/horndis|HoRNDIS]], HoRNDIS (pronounce: “horrendous”) is a driver for Mac OS X that allows you to use your RNDIS to get networ access to Pluto. It is known to work with Mac OS X versions 10.6.8 (Snow Leopard) through 10.12 (Yosemite). Although you should be careful with all drivers that you install on your computer, HoRNDIS has been tested at least well enough for the author (and many others) to run full time on their own personal computers. It would be great if Apple decided to support this natively - since RNDIS is a Microsoft specification, it's unlikely. | * [[http://joshuawise.com/horndis|HoRNDIS]], HoRNDIS (pronounce: “horrendous”) is a driver for Mac OS X that allows you to use your RNDIS to get network access to Pluto. It is known to work with Mac OS X versions 10.6.8 (Snow Leopard) through 10.12 (Yosemite). Although you should be careful with all drivers that you install on your computer, HoRNDIS has been tested at least well enough for the author (and many others) to run full time on their own personal computers. It would be great if Apple decided to support this natively - since RNDIS is a Microsoft specification, it's unlikely. |
| |
The drivers and files should be compatible with: | The drivers and files should be compatible with: |