This is an old revision of the document!
It is recommenced to use the pre-build images, which can be found at github.com/analogdevicesinc/plutosdr-fw/. These are build and tested by Analog Devices, and should work on your PlutoSDR without issues. If you want to change functionality, you will need to follow these instructions. To test your image, it is recommended to use the RAM Boot rather than writing to flash the first time. This keep the default firmware while you are testing your image, so if something goes wrong - its a quick power cycle to fix things.
rgetz@brain:~/github/temp/plutosdr-fw$ grep -i REQUIRED_VIVADO_VERSION $(find ./ -name "adi*.tcl") | grep set set required_vivado_version "2021.1"
This specifies any shell prompt running on your Linux development host
rgetz@brain:~/github/temp/plutosdr-fw$ find /opt/Xilinx/ -name vivado -executable -type f | xargs file | grep ELF /opt/Xilinx/Vivado/2021.2/bin/unwrapped/lnx64.o/vivado: ELF 64-bit LSB executable, x86-64, version 1 (GNU/Linux), dynamically linked, interpreter /lib64/ld-linux-x86-64.so.2, for GNU/Linux 2.6.18, not strippedIf it reports as a 32-bit binary (which the above did not), and you are running on a 64-bit system, do:
michael@HAL9000:~/devel$ dpkg --add-architecture i386 michael@HAL9000:~/devel$ apt-get update michael@HAL9000:~/devel$ sudo apt-get install libc6:i386 libstdc++6:i386
There are a few other tools that are necessary in order to build your own Firmware Image.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel$ sudo apt-get install git build-essential ccache device-tree-compiler dfu-util fakeroot help2man libncurses5-dev libssl1.0-dev mtools rsync u-boot-tools bc python cpio zip unzip file wget
It is recommended that if you are building in a Virtual Machine (which is totally fine), the Base Memory be set to at least 4096 MBytes. The Xilinx Vivado tools require at least 1.6 Gig of memory when compile for the XC7Z010
. It has been reported that 2048 Mbytes is not enough, and will cause the tools to hang.
Starting the build process is just a matter of typing make
within the firmware repository.
The Makefile requires a few environmental variables being set, and of course the ARM GCC toolchain in the PATH.
Some paths maybe adjusted to match your Xilinx Vivado and Vitis install folders.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel$ cd plutosdr-fw or m2k-fw michael@HAL9000:~/devel/plutosdr-fw$ export CROSS_COMPILE=arm-linux-gnueabihf- michael@HAL9000:~/devel/plutosdr-fw$ export PATH=$PATH:/opt/Xilinx/Vitis/2021.2/gnu/aarch32/lin/gcc-arm-linux-gnueabi/bin michael@HAL9000:~/devel/plutosdr-fw$ export VIVADO_SETTINGS=/opt/Xilinx/Vivado/2021.2/settings64.sh michael@HAL9000:~/devel/plutosdr-fw$ make
The initial build takes some time to complete, and also requires an INTERNET connection, since buildroot downloads the source packages from the WEB.
Depending on your distribution, you may need to force Vivado to use Gtk2. You can do that by adding:
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel/plutosdr-fw$ export SWT_GTK3=0
before you type make
.
This specifies any shell prompt running on your Linux development host
michael@HAL9000:~/devel/plutosdr-fw$ ls -AGhl build total 52M -rw-rw-r-- 1 michael 69 Apr 19 17:45 boot.bif -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.bin -rw-rw-r-- 1 michael 446K Apr 19 17:45 boot.dfu -rw-rw-r-- 1 michael 575K Apr 19 17:45 boot.frm -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.dfu -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.frm -rw-rw-r-- 1 michael 33 Apr 19 17:45 pluto.frm.md5 -rw-rw-r-- 1 michael 8,3M Apr 19 17:45 pluto.itb -rw-rw-r-- 1 michael 16M Apr 19 17:45 plutosdr-fw-v0.20.zip -rw-rw-r-- 1 michael 471K Apr 19 17:45 plutosdr-jtag-bootstrap-v0.20.zip -rw-r--r-- 1 michael 4,2M Apr 19 17:39 rootfs.cpio.gz drwxrwxr-x 6 michael 4,0K Apr 19 17:45 sdk -rw-rw-r-- 1 michael 940K Apr 19 17:45 system_top.bit -rw-rw-r-- 1 michael 362K Apr 19 17:45 system_top.hdf -rwxrwxr-x 1 michael 409K Apr 19 17:45 u-boot.elf -rw-rw---- 1 michael 128K Apr 19 17:45 uboot-env.bin -rw-rw---- 1 michael 129K Apr 19 17:45 uboot-env.dfu -rw-rw-r-- 1 michael 4,6K Apr 19 17:45 uboot-env.txt -rwxrwxr-x 1 michael 3,2M Apr 19 17:33 zImage -rw-rw-r-- 1 michael 16K Apr 19 17:39 zynq-pluto-sdr.dtb -rw-rw-r-- 1 michael 16K Apr 19 17:39 zynq-pluto-sdr-revb.dtb
There is a script in the plutosdr_scripts repo that will quickly download a build artifact (the pluto.dfu
file) to an USB attached PlutoSDR. This will load the image into RAM, and not write to flash, enabling easy testing of images. However, since it is loading into RAM, it is not a persistent update over power cycles or further reboots.
This specifies any shell prompt running on your Linux development host
rgetz@brain:~/github/plutosdr-fw$ sudo ../plutosdr_scripts/pluto_ramboot Found Pluto SDR at IP 192.168.3.1, running kernel: Linux pluto 5.4.0-00535-g9c04de11ae53 #1 SMP PREEMPT Fri Aug 20 13:01:03 CEST 2021 armv7l GNU/Linux Found Pluto SDR in dfu mode and downloading ./build/pluto.dfu successfully downloaded Found new PlutoSDR at 192.168.3.1, running kernel: Linux pluto 5.4.0-00535-g9c04de11ae53 #1 SMP PREEMPT Tue Feb 15 16:17:50 EST 2022 armv7l GNU/Linux rgetz@brain:~/github/plutosdr-fw$
File | Comment |
---|---|
pluto.frm | Main PlutoSDR firmware file used with the USB Mass Storage Device |
pluto.dfu | Main PlutoSDR firmware file used in DFU mode |
boot.frm | First and Second Stage Bootloader (u-boot + fsbl + uEnv) used with the USB Mass Storage Device |
boot.dfu | First and Second Stage Bootloader (u-boot + fsbl) used in DFU mode |
uboot-env.dfu | u-boot default environment used in DFU mode |
plutosdr-fw-vX.XX.zip | ZIP archive containg all of the files above |
plutosdr-jtag-bootstrap-vX.XX.zip | ZIP archive containg u-boot and Vivao TCL used for JATG bootstrapping |
File | Comment |
---|---|
boot.bif | Boot Image Format file used to generate the Boot Image |
boot.bin | Final Boot Image |
pluto.frm.md5 | md5sum of the pluto.frm file |
pluto.itb | u-boot Flattened Image Tree |
rootfs.cpio.gz | The Root Filesystem archive |
sdk | Vivado/XSDK Build folder including the FSBL |
system_top.bit | FPGA Bitstream (from HDF) |
system_top.hdf | FPGA Hardware Description File exported by Vivado |
u-boot.elf | u-boot ELF Binary |
uboot-env.bin | u-boot default environment in binary format created form uboot-env.txt |
uboot-env.txt | u-boot default environment in human readable text format |
zImage | Compressed Linux Kernel Image |
zynq-pluto-sdr.dtb | Device Tree Blob for Rev.A |
zynq-pluto-sdr-revb.dtb | Device Tree Blob for Rev.B |
Function | File |
---|---|
PlutoSDR Linux Kernel Config | zynq_pluto_defconfig |
make -C linux ARCH=arm zynq_pluto_defconfig make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zImage UIMAGE_LOADADDR=0x8000 cp linux/arch/arm/boot/zImage build/zImage
Normal users should not need to change their kernel, and this is only described for advanced users, or developers who periodically forget things
The command
make -C linux ARCH=arm zynq_pluto_defconfig
copies the file from arch/arm/configs/zynq_pluto_defconfig
to .config
and
make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zImage UIMAGE_LOADADDR=0x8000
builds it.
If you want to make a custom kernel, the easiest thing to do, is modify the .config
with
make -C linux ARCH=arm zynq_pluto_defconfig make -C linux ARCH=arm menuconfig
and then make changes, save them, and then create the defconfig
.
make -C linux ARCH=arm savedefconfig
Check your changes against the default image
diff -u ./linux/arch/arm/configs/zynq_pluto_defconfig linux/defconfig | less
And if you are sure things are what you want, store them to the default file.
cp ./linux/defconfig ./linux/arch/arm/configs/zynq_pluto_defconfig
then this will work next time you type make
to build the firmware image.
Function | File |
---|---|
PlutoSDR Rev.A Device Tree | zynq-pluto-sdr.dts |
PlutoSDR Rev.B Device Tree | zynq-pluto-sdr-revb.dts |
make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr.dtb cp linux/arch/arm/boot/dts/zynq-pluto-sdr.dtb build/zynq-pluto-sdr.dtb make -C linux -j 8 ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- zynq-pluto-sdr-revb.dtb cp linux/arch/arm/boot/dts/zynq-pluto-sdr-revb.dtb build/zynq-pluto-sdr-revb.dtb
Function | File |
---|---|
PlutoSDR Buildroot Config | zynq_pluto_defconfig |
make -C buildroot ARCH=arm zynq_pluto_defconfig make -C buildroot TOOLCHAIN_EXTERNAL_INSTALL_DIR= ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- BUSYBOX_CONFIG_FILE=/home/michael/devel/pluto/plutosdr-fw/buildroot/board/pluto/busybox-1.25.0.config all cp buildroot/output/images/rootfs.cpio.gz build/rootfs.cpio.gz
You need to copy over the correct file, to the .config
, edit it (with menuconfig
), and then save it to the right place so that the main build system will use the new file.
make -C buildroot ARCH=arm zynq_pluto_defconfig make -C buildroot ARCH=arm menuconfig make -C buildroot ARCH=arm savedefconfig make
Function | File |
---|---|
Pluto HDL Project | Files |
source /opt/Xilinx/Vivado/2021.2/settings64.sh make -C hdl/projects/pluto cp hdl/projects/pluto/pluto.sdk/system_top.hdf build/system_top.hdf
Function | File |
---|---|
Create FSBL TCL script | create_fsbl_project.tcl |
source /opt/Xilinx/Vivado/2021.2/settings64.sh xsdk -batch -source scripts/create_fsbl_project.tcl cp build/sdk/hw_0/system_top.bit build/system_top.bit
Function | File |
---|---|
PlutoSDR Image Tree Source | pluto.its |
u-boot-xlnx/tools/mkimage -f scripts/pluto.its build/pluto.itb
cp build/pluto.itb build/pluto.itb.tmp dfu-suffix -a build/pluto.itb.tmp -v 0x0456 -p 0xb673 mv build/pluto.itb.tmp build/pluto.dfu
md5sum build/pluto.itb | cut -d ' ' -f 1 > build/pluto.frm.md5 cat build/pluto.itb build/pluto.frm.md5 > build/pluto.frm
Function | File |
---|---|
PlutoSDR u-boot Config | zynq_pluto_defconfig |
PlutoSDR u-boot Device Tree | zynq-pluto-sdr.dts |
make -C u-boot-xlnx ARCH=arm zynq_pluto_defconfig make -C u-boot-xlnx ARCH=arm CROSS_COMPILE=arm-xilinx-linux-gnueabi- UBOOTVERSION="PlutoSDR v0.20-PlutoSDR" cp u-boot-xlnx/u-boot build/u-boot.elf
echo img:{[bootloader] build/sdk/fsbl/Release/fsbl.elf build/u-boot.elf } > build/boot.bif source /opt/Xilinx/Vivado/2021.2/settings64.sh bootgen -image build/boot.bif -w -o build/boot.bin
cp build/boot.bin build/boot.bin.tmp dfu-suffix -a build/boot.bin.tmp -v 0x0456 -p 0xb673 mv build/boot.bin.tmp build/boot.dfu
CROSS_COMPILE=arm-xilinx-linux-gnueabi- scripts/get_default_envs.sh > build/uboot-env.txt u-boot-xlnx/tools/mkenvimage -s 0x20000 -o build/uboot-env.bin build/uboot-env.txt
cp build/uboot-env.bin build/uboot-env.bin.tmp dfu-suffix -a build/uboot-env.bin.tmp -v 0x0456 -p 0xb673 mv build/uboot-env.bin.tmp build/uboot-env.dfu
cat build/boot.bin build/uboot-env.bin scripts/target_mtd_info.key | tee build/boot.frm | md5sum | cut -d ' ' -f1 | tee -a build/boot.frm