There are few different use cases, and methods to locally (USB/Serial), or remotely (USB/Network) to reboot a Pluto/M2k.
Pluto/M2k was designed never to have to be rebooted - but software bugs happen. Before you reboot things - try to ask yourself “why”, what went wrong, how do I reproduce, and how can I file a bug report that will help someone debug.
Welcome to: ______ _ _ _________________ | ___ \ | | | / ___| _ \ ___ \ | |_/ / |_ _| |_ ___ \ `--.| | | | |_/ / | __/| | | | | __/ _ \ `--. \ | | | / | | | | |_| | || (_) /\__/ / |/ /| |\ \ \_| |_|\__,_|\__\___/\____/|___/ \_| \_| v0.20 http://wiki.analog.com/university/tools/pluto # device_reboot Usage: /usr/sbin/device_reboot {ram|sf|reset|verbose|break} sf : Reboot and enter Serial Flash DFU mode ram : Reboot and enter RAM DFU mode reset : Reboot verbose: Reboot and start serial console Verbose break : Reboot and HALT in u-boot #
# device_reboot ram Stopping input-event-daemon: done Stopping dropbear sshd: OK Stopping MSD Daemon: OK Stopping dhcpd Daemon & httpd Server: FAIL Stopping network: OK Stopping system message bus: done Stopping UDC Gadgets configfs-gadget gadget: unbind function 'rndis'/cbcaa480 configfs-gadget gadget: unbind function 'Mass Storage Function'/cbc4e9c0 configfs-gadget gadget: unbind function 'acm'/cc35e000 configfs-gadget gadget: unbind function 'Function FS Gadget'/cc35e9e4 Stopping logging: OK umount: devtmpfs busy - remounted read-only umount: can't unmount /: Invalid argument The system is going down NOW! Sent SIGTERM to all processes Sent SIGKILL to all processes Requesting system reboot reboot: Restarting system U-Boot PlutoSDR v0.20-PlutoSDR-00041-g4bdff59 (Apr 19 2017 - 17:45:50 +0200) I2C: ready DRAM: ECC disabled 512 MiB SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Model: Zynq Pluto SDR Board Hit any key to stop autoboot: 0 Entering DFU RAM mode … Copying Linux from DFU to RAM…
This specifies any shell prompt running on the development host
Following commands can be used to boot a fresh build of the firmware image. To simply things, there is a script in plutosdr_scripts pluto_ramboot
that can do all these steps in one command.
sshpass -p analog ssh root@pluto '/usr/sbin/pluto_reboot ram;' sleep 5 sudo dfu-util -l dfu-util 0.9 Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc. Copyright 2010-2016 Tormod Volden and Stefan Schmidt This program is Free Software and has ABSOLUTELY NO WARRANTY Please report bugs to http://sourceforge.net/p/dfu-util/tickets/ Found DFU: [0456:b674] ver=0221, devnum=11, cfg=1, intf=0, path="1-4", alt=1, name="firmware.dfu", serial="UNKNOWN" Found DFU: [0456:b674] ver=0221, devnum=11, cfg=1, intf=0, path="1-4", alt=0, name="dummy.dfu", serial="UNKNOWN" sudo dfu-util -d 0456:b673,0456:b674 -D ./build/pluto.dfu -a firmware.dfu sudo dfu-util -d 0456:b673,0456:b674 -a firmware.dfu -e
# device_reboot sf Stopping input-event-daemon: done Stopping dropbear sshd: OK Stopping MSD Daemon: OK Stopping dhcpd Daemon & httpd Server: FAIL Stopping network: OK Stopping system message bus: done Stopping UDC Gadgets configfs-gadget gadget: unbind function 'rndis'/df624600 configfs-gadget gadget: unbind function 'Mass Storage Function'/cbc13600 configfs-gadget gadget: unbind function 'acm'/cbc12780 configfs-gadget gadget: unbind function 'Function FS Gadget'/cbc4e9e4 Stopping logging: OK umount: devtmpfs busy - remounted read-only umount: can't unmount /: Invalid argument The system is going down NOW! Sent SIGTERM to all processes Sent SIGKILL to all processes Requesting system reboot reboot: Restarting system U-Boot PlutoSDR v0.20-PlutoSDR-00041-g4bdff59 (Apr 19 2017 - 17:45:50 +0200) I2C: ready DRAM: ECC disabled 512 MiB SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Model: Zynq Pluto SDR Board Hit any key to stop autoboot: 0 Entering DFU SF mode … SF: Detected N25Q256A with page size 256 Bytes, erase size 4 KiB, total 32 MiB
# reboot