This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy [04 May 2018 11:48] – Antoniu Miclaus | university:tools:m2k:scopy [28 Sep 2022 22:11] (current) – [Download] Adrian Suciu | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== About ===== | ===== About ===== | ||
- | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. | + | Scopy is a multi-functional software toolset with strong capabilities for signal analysis. |
===== Download ===== | ===== Download ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | * **Scopy for Windows | + | |
- | * Download: [[https:// | + | **Scopy for Windows ** |
- | * Download: [[https://ci.appveyor.com/api/projects/ | + | * Download: [[https:// |
+ | |||
+ | **Scopy for Linux ** | ||
+ | * Download: [[https://github.com/analogdevicesinc/scopy/ | ||
+ | |||
+ | **Scopy for OSX ** | ||
+ | * Download: [[https:// | ||
+ | |||
+ | **Scopy for Android ** | ||
+ | * Download: [[https:// | ||
+ | * Google Play store link: [[https:// | ||
+ | |||
+ | **Scopy all platforms latest(nightly) builds ** | ||
+ | * Download: [[https:// | ||
</ | </ | ||
- | <WRAP round important> | + | |
- | * [[university: | + | <WRAP round important> |
+ | * [[university: | ||
</ | </ | ||
===== Installation ===== | ===== Installation ===== | ||
+ | |||
+ | === Scopy for Windows === | ||
Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | Once you downloaded the installer, run it and follow all the required steps. After completion, system reboot is required. | ||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for Linux === | ||
+ | Before downloading and extracting the scopy-v1.1.1-Linux-flatpak.zip archive, you need to setup Flatpak using [[https:// | ||
+ | |||
+ | For Ubuntu, you can use the following steps: | ||
+ | < | ||
+ | **sudo add-apt-repository ppa: | ||
+ | sudo apt update | ||
+ | sudo apt install flatpak | ||
+ | flatpak remote-add --if-not-exists flathub https:// | ||
+ | </ | ||
+ | |||
+ | After this, get the **Scopy.flatpak** file from the downloaded archive and run: | ||
+ | |||
+ | < | ||
+ | **flatpak install scopy-v1.1.1-Linux-flatpak.flatpak** | ||
+ | </ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for OSX === | ||
+ | Double click the downloaded .dmg to make its content available. " | ||
+ | Drag the application from the .dmg window into Applications to install and wait for the process to finish. \\ | ||
+ | |||
+ | === Video === | ||
+ | {{youtube> | ||
+ | \\ | ||
+ | === Scopy for Android === | ||
+ | Tap on the downloaded .apk file to start the installation process and proceed by hitting the " | ||
+ | In order to connect [[adi> | ||
+ | \\ | ||
+ | <WRAP centeralign> | ||
+ | \\ | ||
+ | |||
===== Launching ===== | ===== Launching ===== | ||
- | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder | + | Run Scopy from the Desktop Shortcut / Start Menu / Installation Folder. \\ |
+ | |||
+ | On Linux, you can also run it using: | ||
+ | < | ||
+ | **flatpak run org.adi.Scopy** | ||
+ | </ | ||
====== Using the Application ===== | ====== Using the Application ===== | ||
Line 22: | Line 81: | ||
===== Home ===== | ===== Home ===== | ||
- | The Home view is divided into three sections: | + | The Home view is divided into four sections: |
- | * **Devices**: | + | * **Devices(1)**: List of devices (USB or remote) that Scopy can connect to. USB devices are detected automatically at startup. The __Add__ button can be used to add remote devices to the list. |
- | * **Instruments Menu**: List with instruments provided by the application. | + | * **Instruments Menu(2)**: List with instruments provided by the application. |
- | * **Information Window**: | + | * **Information Window(3)**: Section containing the welcome, add device |
+ | * **General Settings Menu(4)**: Save and load session and the preferences menu. | ||
- | {{ : | + | <WRAP centeralign> |
+ | </ | ||
- | \\ | ||
==== Connecting to a USB device ==== | ==== Connecting to a USB device ==== | ||
- | If a compatible USB device is available it will be displayed | + | If a compatible USB device is available it will be displayed |
- | To connect to that device click on the device and then click the **Connect** button. If the connection was established, | + | |
- | {{ : | + | To connect to that device click on the device and then click the **Connect** button in the **Information Window**. |
+ | |||
+ | If the connection was established, | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
- | \\ | ||
==== Connecting to a remote device ==== | ==== Connecting to a remote device ==== | ||
To connect to a remote device click on the **Plus** icon. Enter the IP of the remote device into the **Hostname** field and click the **Connect** button. If a device can be detected at the IP you provided, the **Connect** button will change to an **Add** button and you can click on it to add the remote device to the list of detected devices. | To connect to a remote device click on the **Plus** icon. Enter the IP of the remote device into the **Hostname** field and click the **Connect** button. If a device can be detected at the IP you provided, the **Connect** button will change to an **Add** button and you can click on it to add the remote device to the list of detected devices. | ||
- | The last step is to click on the icon of the remote device and click on the **Connect** button. | + | \\ |
+ | <WRAP centeralign> | ||
+ | </ | ||
- | {{ : | + | <WRAP centeralign> |
+ | </ | ||
+ | |||
+ | Clicking the **Forget Device** button will remove the device from the list. | ||
+ | Clicking the **Identify** button will make the device blink. | ||
\\ | \\ | ||
- | ===== Instruments Menu ===== | ||
- | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, | + | ===== General Settings Menu ===== |
- | The icon on the right of the instrument name specifies that the instrument is enabled and provides a shortcut that allows an instrument to be turned on or off. | + | |
- | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. | + | <WRAP centeralign> |
- | {{ : | + | </ |
- | \\ | + | The save/load buttons can be used to save the current session or load another session. |
- | ===== Digital IO ===== | + | The preferences button will open the preferences for Scopy where different options for different tools can be modified. |
- | Digital IO details are available [[university: | + | <WRAP centeralign> |
+ | </ | ||
- | \\ | + | Clicking the **Reset Scopy** button will reset the application to a default configuration. |
- | ===== Voltmeter ===== | + | Checking the **user notes preference** will enable a tool where the user can add different pages with html formatted text |
- | Voltmeter details are available [[university: | + | <WRAP centeralign> |
+ | </ | ||
\\ | \\ | ||
- | ===== Oscilloscope | + | ===== User Guides |
- | Oscilloscope details are available [[university: | + | |
- | \\ | + | Scopy interacts with only one hardware device at a time. Once a device is selected to be used with the application, |
- | ===== Signal Generator ===== | + | The icon on the right of the instrument name specifies that the instrument is enabled and provides a shortcut that allows an instrument to be turned on or off. |
- | Signal Generator details | + | |
- | \\ | + | The instruments menu can be minimized by clicking on the **Scopy** button near the top-left window. |
- | ===== Power Supply ===== | + | |
- | Power Supply details are available [[university: | + | |
- | \\ | + | <WRAP centeralign> |
- | ===== Pattern Generator ===== | + | </ |
- | Pattern Generator details are available [[university: | + | |
- | \\ | + | === Detaching Instruments === |
- | ===== Logic Analyzer ===== | + | Scopy provides the detaching into multiple windows feature for each instrument |
- | Logic Analyzer details are available | + | |
- | \\ | + | There are 2 ways to do this: |
+ | - __Drag and Drop__ - select the desired instrument drag it outside Instrument Menu section and drop it inside the application window area. | ||
- | ===== Network Analyzer ===== | + | <WRAP centeralign> |
- | Network Analyzer details are available [[university: | + | </ |
+ | |||
+ | - __Double Click__ - first make sure that the **Double click to detach a tool** option is enabled in the **Preferences** menu; double-click on the desired instrument to detach it. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | </ | ||
\\ | \\ | ||
- | ===== Spectrum Analyzer | + | ==== Instruments Overview==== |
- | Spectrum Analyzer details are available [[university: | + | |
+ | <WRAP centeralign> | ||
+ | </ | ||
+ | |||
+ | Complete user guides on how to use each Scopy instrument: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | - [[university: | ||
+ | |||
+ | ==== Scripts ==== | ||
+ | |||
+ | User guide on how to use scripts with Scopy: | ||
+ | * [[university: | ||
\\ | \\ | ||
====== Building ====== | ====== Building ====== | ||
- | ===== Linux ===== | + | |
- | For building | + | Complete |
- | \\ | + | - [[university: |
- | ===== Windows ===== | + | - [[university: |
- | For building Scopy on Windows, use the steps defined | + | |
Line 107: | Line 193: | ||
====== Source code ====== | ====== Source code ====== | ||
- | The source code for the entire application | + | The source code for the entire application |