This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:m2k:scopy:voltmeter [11 Sep 2017 08:06] – Updated the picture in accordance to the latest version of Voltmeter. Dann Kristofer Bautista | university:tools:m2k:scopy:voltmeter [07 Apr 2021 22:10] (current) – adding video Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Scopy Voltmeter ====== | ====== Scopy Voltmeter ====== | ||
+ | |||
+ | ===== Video ===== | ||
+ | {{youtube> | ||
===== General Description ===== | ===== General Description ===== | ||
Line 5: | Line 8: | ||
Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. | Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. | ||
- | The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±20V. | + | The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±25V. |
<WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary. | <WRAP round info 65%>A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary. | ||
</ | </ | ||
- | {{: | ||
==== Main Window ==== | ==== Main Window ==== | ||
+ | |||
+ | {{ : | ||
==== History Plot ==== | ==== History Plot ==== | ||
Line 20: | Line 24: | ||
\\ | \\ | ||
\\ | \\ | ||
- | {{ : | ||
==== Run/Stop Button ==== | ==== Run/Stop Button ==== | ||
The Run/Stop Button on the top-right corner of the Scopy window can be used to start and stop the capture for the two channels. Stopping the capture saves the last reading for both channels. | The Run/Stop Button on the top-right corner of the Scopy window can be used to start and stop the capture for the two channels. Stopping the capture saves the last reading for both channels. | ||
Alternatively, | Alternatively, | ||
+ | |||
+ | {{: | ||
+ | |||
\\ | \\ | ||
\\ | \\ | ||
==== AC/DC Modes ==== | ==== AC/DC Modes ==== | ||
+ | {{ : | ||
AC/DC mode may be set independently for each channel. AC Mode will display the VRMS value of the signal and is optimized for frequencies between 20Hz to 40kHz, this range of frequency is separated in two options. | AC/DC mode may be set independently for each channel. AC Mode will display the VRMS value of the signal and is optimized for frequencies between 20Hz to 40kHz, this range of frequency is separated in two options. | ||
\\ | \\ | ||
- | {{: | ||
\\ | \\ | ||
The first option is frequency range from 20Hz to 800Hz and the second option is from 800Hz to 40kHz. When the signal’s frequency is not within the range of the option selected, there will be no reading in the instrument. | The first option is frequency range from 20Hz to 800Hz and the second option is from 800Hz to 40kHz. When the signal’s frequency is not within the range of the option selected, there will be no reading in the instrument. | ||
\\ | \\ | ||
\\ | \\ | ||
- | DC Mode will display the VDC value of the signal from -20V to 20V. | + | DC Mode will display the VDC value of the signal from -25V to 25V. |
\\ | \\ | ||
\\ | \\ | ||
==== History ==== | ==== History ==== | ||
+ | {{ : | ||
The Voltmeter features one Voltage-over-time history plot per channel. These can be independently enabled and disabled by toggling the ON/OFF switches on the right-side menu. | The Voltmeter features one Voltage-over-time history plot per channel. These can be independently enabled and disabled by toggling the ON/OFF switches on the right-side menu. | ||
There' | There' | ||
\\ | \\ | ||
- | {{: | ||
\\ | \\ | ||
By default, the plot will represent 10 seconds of data. This selector will allow you to choose the history duration between the three choices: 1 second, 10 seconds, 60 seconds. | By default, the plot will represent 10 seconds of data. This selector will allow you to choose the history duration between the three choices: 1 second, 10 seconds, 60 seconds. | ||
\\ | \\ | ||
\\ | \\ | ||
+ | \\ | ||
+ | ==== Data logging ==== | ||
+ | {{ : | ||
+ | The data logging can be enabled or disabled using the ON/OFF switch in the right-side menu. A file can be chosen clicking the **Browse** button | ||
+ | \\ | ||
+ | \\ | ||
+ | The Voltmeter can Overwrite or Append to the selected file by checking one of the options located below the file selector. | ||
+ | \\ | ||
+ | \\ | ||
+ | The timer control, located at the bottom of the right-side menu, controls the amount of data that will be logged. The accepted range of values for this control is between 0 seconds and 1 hour. By default, the spinbox is set to 0. In this case, each value displayed on the LCD will be written to the selected file. If the value is, for example, 4, the Voltmeter will log to file every 4 seconds. | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | |||
+ | ==== Peak hold==== | ||
+ | |||
+ | The peak hold functionality can be enabled or disabled using the ON/OFF switch in the right-side menu. | ||
+ | |||
+ | The min and max values are visible on the digital display and can be reset using the **Reset** button. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | \\ | ||
+ | |||
**Return to [[university: | **Return to [[university: | ||