This is an old revision of the document!
The voltmeter instrument displays the voltage readings on the two channels of the ADC.
Open the Voltmeter instrument by clicking on the “Voltmeter” button displayed at the far left of the Scopy window. The voltmeter instrument makes use of the Oscilloscope probes 1 and 2 in the M2k for the channels which are capable of measuring DC and AC signals at ±20V.
A Calibration feature automatically starts for the Voltmeter instrument when Scopy connects to an M2k device. Manual calibration is not necessary.
The graphical representation of the voltage value over time for each channel is displayed. The history plot is in the form of a strip chart where the voltage amplitude is plotted on the x-axis and time is plotted on the y-axis. This may be turned off in the control menu.
The numerical value representation of the voltage reading on both channels are displayed present in this section. The voltage value displayed may either be in VDC in Direct Current mode or Vrms in AC Mode.
The Run/Stop Button on the top-right corner of the Scopy window can be used to start and stop the capture for the two channels. Stopping the capture saves the last reading for both channels.
Alternatively, the capture can be started and stopped by clicking on the small white square at the right of the instrument name in the left side menu.
AC/DC mode may be set independently for each channel. AC Mode will display the VRMS value of the signal and is optimized for frequencies between 20Hz to 40kHz, this range of frequency is separated in two options.
The first option is frequency range from 20Hz to 800Hz and the second option is from 800Hz to 40kHz. When the signal’s frequency is not within the range of the option selected, there will be no reading in the instrument.
DC Mode will display the VDC value of the signal from -20V to 20V.
The Voltmeter features one Voltage-over-time history plot per channel. These can be independently enabled and disabled by toggling the ON/OFF switches on the right-side menu.
There's a selector below the ON/OFF switches.
By default, the plot will represent 10 seconds of data. This selector will allow you to choose the history duration between the three choices: 1 second, 10 seconds, 60 seconds.
Return to Scopy Main Page