This is an old revision of the document!
Make sure you install the latest driver -
Some USB cables are incapable of power delivery necessary to the ADALM2000 (or are just plain flakey). Please use the provided USB cable. Also in order to troubleshoot this, you try using two cables, plug in a separate cable to the USB connector for power delivery (to the USB power connector), while using the center USB connector for data transfer. If using two cables works, it normally means it's a cable, or voltage droop issue on the host.
Scopy.ini
and Preferences.ini
contain the user-settings that are saved in-between sessions. Sometimes these can get messed up and can cause problems. In order to reset them, go to:
These file are located in:
C:\Users\<your_username>\AppData\Roaming\ADI
Sometimes this is a hidden directory, and you unhide it./home/<your_username>/.config/ADI
/Users/<your_username>/.config/analog.com
and delete (or rename) Scopy.ini
, Scopy.ini.bak
, Preferences.ini
, Preferences.ini.bak
. The preference is to rename things with a different suffix, so if you need to report a bug, the file still exists.
If you are having trouble connecting through USB, you can always connect to the ADALM2000 through the network interface. The USB connection can cause all kinds of problems on various systems. In order to connect through the emulated network interface follow these steps.
Visit the ADALM2000 firmware page https://github.com/analogdevicesinc/m2k-fw/releases.
Compare the latest firmware version on this page with the one you have installed. Follow these steps to update the firmware.
Download latest version of https://github.com/analogdevicesinc/libiio/releases .
Open a command prompt and run
iio_info -a
or
iio_info -u "ip:192.168.2.1"